Targeting High-End Navigation Systems, the R-Car H1 Enables a Complete Solution for the Next-Generation Systems

October 18, 2011

TOKYO, Japan, October 18, 2011 — Renesas Electronics Corporation (TSE: 6723) and its subsidiary, Renesas Mobile Corporation, today announced a new member of the R-Car series of automotive systems-on-chip (SoCs), the R-Car H1, capable of delivering up to 11,650 Dhrystone MIPS (DMIPS), and ideal for the high-end car navigation market. The R-Car H1 SoC offers an innovative architecture where the application domain is powered by an ARM® Cortex™A-9 quad-core configuration running at 1 gigahertz (GHz), while the real-time domain is powered by a dedicated multimedia engine (MME) based on Renesas' SH4A core. The R-Car's architecture allows customers to implement features such as quick-boot, backup camera support and media processing using the MME, while the application domain cores can be allocated to run advanced operating systems such as Linux, Windows® Automotive Embedded or QNX®.

Renesas' R-Car H1 SoC offers one of the most complete system integrations on the market available today. Powered with Imagination Technologies' SGX-543-MP2 graphics processing unit (GPU), and delivering up to 40 gigaflops per second (Gflops/s, effective), the R-Car H1 SoC offers one of the best graphical performances in the embedded market. The GPU is ready to support open technologies OpenGL ES 2.0 and OpenVG 1.1, making it a perfect platform to develop next-generation car infotainment systems.

The R-Car H1 SoC is also powered (as an optional feature) with Renesas' IMP-X3 core, a real-time image processing unit that enables developers with the emerging trend of augmented reality. To fully benefit from the IMP-X3 core, the R-Car H1 SoC also supports up to four independent input camera channels allowing easy implementation of 360-degree camera views and sign recognition to mention a few applications.

Video and audio processing is supported by hardware accelerators supporting up to HD 1080p @ 60fps on advanced infotainment systems. To insure adequate memory bandwidth, the R-Car H1 SoC is equipped with two independent DDR3 32-bit interfaces which allow access to different content simultaneously, providing higher performance when compared to solutions that offer a single 64-bit DDR interface.

The R-Car H1 integrated peripherals include Ethernet, MOST-150, PATA and SATA interfaces and PCIe for system expansion. The R-Car H1 SoC also offers a version with a GPS baseband engine enabling further system integration. The R-Car Series offers multiple CAN channels and two independent display controllers as well as three USB 2.0 ports with PHY.

Availability

Samples of Renesas' R-Car H1 SoCs will be available starting in November 2011, equipped in an 832-pin FCBGA (flip chip ball grid array) package, and its pricing is to be decided. Mass production is scheduled to begin in December 2012 and is expected to reach a cumulative 100,000 units per month in December 2013. (Availability is subject to change without notice.)

Refer to the separate sheet for product specifications

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.

(Remarks) ARM and Cortex are registered trademarks or trademarks of ARM Limited. PowerVR SGX is a registered trademark of Imagination Technologies in the EU and other countries. QNX is a registered trademark of QNX Software Systems. Windows is a registered trademark of Microsoft Corporation. Other product and service names that appear in this press release are trademarks or registered trademarks of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

Share this news on