Renesas Electronics Announces Power Semiconductor Devices with Large-Current and Low Power Loss for Consumer Motor Drive Applications

Contribute to Longer Battery Life for Power Tools and Power-Assisted Bicycles

19 Jul 2011

TOKYO, Japan, July 19, 2011 — Renesas Electronics Corporation (TSE: 6723), a premier provider of advanced semiconductor solutions, today announced the development of 100 ampere (A) high-current power MOSFETs for motor drive in consumer products, such as cordless power tools and power-assisted bicycles, as part of a wider effort to strengthen the company's entire line of power semiconductor devices. The new power MOSFETs cover a wide range of voltages, with three new products, including the N0413N, having a voltage tolerance of 40 V and three others, including the N0601N, having a voltage tolerance of 60 V. The new power MOSFETs have loss levels among the lowest in the industry, making them ideal for extending battery life.

In recent years the market for cordless power tools has seen an increase, especially among high-end models, in the use of brushless motors and other power efficiency measures to increase battery life. The power supply circuit of a typical power tool contains six power MOSFET devices, and there is increasing demand for power MOSFETs with low-loss characteristics (low on-resistance*).

Renesas Electronics has many years of experience in developing power semiconductor devices, and currently mass produces low-loss, high-performance power MOSFET products for the consumer, industrial, automotive, and other fields. The company's lineup of consumer power MOSFETs previously extended only to a current rating of 83 A. In response to the above-mentioned increase in demand for power semiconductor devices for use in cordless power tools, Renesas Electronics has developed six new low-loss power MOSFETs designed to accommodate large currents up to 100 A.

Key features of the new power MOSFET devices:

  • (1) High-current and low-loss characteristics for extended battery life in products such as cordless power tools

The new power MOSFETs use measures such as innovative mounting technology to accommodate large currents up to 100 A, making them suitable for use in applications such as cordless power tools. In addition, they deliver low-loss characteristics among the best in the industry through the use of design technology built up over many years. For example, the N0413N with 40 V voltage tolerance has an on-resistance (Ron) of only 2.7 mΩ, and the N0601N with 60 V voltage tolerance has an on-resistance (Ron) of only 3.3 mΩ (VGSS = 10 V standard value in both cases). This contributes to longer battery life.

 

  • (2) Wide voltage range and support for many mounting configurations

The new products are available with a voltage tolerance of 40 V or 60 V and in three package types, the TO-220AB and TO-262 and the surface-mount TO-263, for a total of six versions. Customers can choose the voltage tolerance and package that best match their application.

 

Renesas continues to aggressively expand its lineup of power MOSFET products to best address the changing requirements of a variety of applications.

 

Please refer to the separate sheet for the specifications of the new power MOSFETs.

 

Pricing and Availability

Samples of the new power MOSFET devices are available now, priced at US$1.2 per unit. Mass production is scheduled to begin in August 2011, and is expected to reach a scale of 2 million units per month, for all six products combined, by the latter half of FY2012.
(Pricing and availability are subject to change without notice.)

 

(Remarks)

All other registered trademarks or trademarks are the property of their respective owners. 

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power, and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.