Low-end USB Microcontrollers Designed for Consumer and Healthcare Devices

December 9, 2010

TOKYO, December 9, 2010 — Renesas Electronics Corporation (TSE: 6723), a premier supplier of advanced semiconductor solutions, today introduced its first low-end flash microcontrollers (MCUs) with a built-in Universal Serial Bus 2.0 (USB) host/function controller, designed for consumer electronics such as PC peripherals, mobile devices, and healthcare equipment. The new MCU products are part of the R8C Family, and include the R8C/34K and R8C/3MK Groups, which incorporate a USB host/function controller, and the R8C/34U and R8C/3MU Groups with a USB function-only controller.

Taking advantage of its proven track record for mid- to high-end MCUs with built-in USB controllers, Renesas Electronics has responded to market needs by releasing new low-end MCUs that incorporate a USB host/function controller. In the R8C/34K Group of MCUs, the USB peripheral also can be configured for On-The-Go (OTG) functionality to provide greater flexibility and simplify system design. The new devices offer variants ranging from 32 to 128 kilobytes (KB) with up to 10KB of SRAM, and 4KB of data flash for data storage, and are offered in a 7×7 millimeter (mm) or 6×6 mm package.

Following are key features of the new USB MCUs:

(1) High-functionality USB host/function controller

The USB controller conforms to the USB 2.0 full-speed (12 Mbps) specifications. Furthermore, the controller consists of five high-performance and flexible communication pipes, and each pipe includes its own FIFO memory (for a total of 448 bytes). Thus, applications can select double or single buffering and the communication direction according to the needs of the system application in software.

When this USB controller is used as a host, it can achieve highly efficient USB communication by automatically repeating transfers using the free time in the USB frame. Also, since the transfer scheduling is performed in hardware, the CPU load is reduced significantly.

When this USB controller is used as a USB function controller, it performs the state management required for USB communication and the control transfer stage management in hardware. This means that communication with a USB host can be implemented with even simpler software, thereby reducing development time. Since this USB controller includes a USB power supply regulator, a single-voltage power supply (3.0 to 5.5 volts) provided by the USB cable can be utilized to minimize system cost.

The R8C/34K Group products allow the USB host and USB function operations to be switched with register settings and can also support USB OTG.

(2) Support for a wide range of low-power modes

Just as the existing R8C/3x Series does, the new MCUs provide both wait mode and stop mode, which significantly reduce power consumption. Furthermore, the internal PLL circuit for the USB clock can be disabled when the USB is not required, to reduce the power consumption even more.

(3) Compact package

The new R8C/34K and R8C/34U Group MCUs, and the R8C/3MK and R8C/3MU Group MCUs, come in a 7×7 mm 48-pin LQFP package and a 6×6 mm 40-pin QFN package respectively, allowing system designers to select the best package for the application system.

Pricing and Availability

Samples of Renesas Electronics' new MCUs are available now. The sample prices of these new MCUs vary depending on memory capacity and package. For example, the R5F2134CKNFP MCU with 128 kilobytes (KB) of flash memory and 10 KB of RAM in a 48-pin LQFP package is priced at US$6 per unit. Mass production is scheduled to begin in March 2011 and is expected to reach a combined volume of 500,000 units per month by March 2012. (Pricing and availability are subject to change without notice.)

Please refer to the separate sheet for the main specifications of the new USB MCUs.

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.

(Remarks) All product and service names that appear in this press release are trademarks or registered trademarks of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

Share this news on