Renesas Electronics Introduces Three New SoCs for USB/SD Audio Decoders with 88 Percent Reduced Package Size

02 Dec 2010

TOKYO, Japan, December 2, 2010 — Renesas Electronics Corporation (TSE: 6723), a premier provider of advanced semiconductor solutions, today announced the availability of three new audio decoder systems-on-chip (SoCs), the µPD63530, µPD63910 and µPD63911, with an integrated USB (Universal Serial Bus) host controller.

The new SoCs are ideal for use in automotive and consumer products. The µPD63530 device is available in a 48-pin low-profile quad flat-pack (LQFP) package that is 88 percent smaller than existing package offerings. The µPD63910 and µPD63530 SoCs allow easy software upgrading through the use of external flash memory. In addition to a host controller supporting USB 2.0 (full speed, 12 megabits per second (Mbps)), the new devices integrate all the functions needed in a audio system to decode music in three popular formats: MP3, Windows Media Audio™ (WMA), and AAC.

System features of the new Renesas Electronics SoCs will shorten the amount of time needed to develop audio systems that play audio data stored on USB memory devices or Secure Digital (SD) cards.

Key features of the new products:

  • (1) 88 percent smaller package (µPD63530) 

    The new SoCs are equipped in a compact 48-pin LQFP package (7 millimeter (mm) × 7 mm), which is an 88 percent smaller package than the company's existing package offerings.


  • (2) Easy updating of software by using external flash memory (µPD63910 and µPD63530) 

    Renesas Electronics' new SoCs simplify software updates by allowing the designer to store modified versions of the system firmware in external memory. These updates are uploaded to the SoCs at boot time, allowing for future enhancement of system functions.


  • (3) Wide range of USB solutions in one package 

    The new devices incorporate a USB host controller (including on-chip PHY), and functions for decoding compressed audio data. All the functions required to play audio files stored on a USB memory device, SD card, or digital music player are provided in a single chip.


  • (4) Built in software for USB decoding 

    The standard integrated software includes USB control; MP3, WMA and AAC decoding functions; a WAV file playback function; file system control; and system control functions. Customers can develop application software running on their host processor that simply issues control commands (Play, Stop, etc), substantially reducing the amount of development time required.

 

More information can be found on the separate sheet for the specifications of the new SoCs, the µPD63530, µPD63910 and µPD63911.

 

Exhibition at Embedded Technology 2010

Renesas Electronics' new SoCs will be showcased in the company's booth at the Embedded Technology (ET) 2010, to be held in Yokohama, Japan, from December 1 to 3.

 

Pricing and Availability

Samples of Renesas Electronics' new SoCs (part numbers µPD63530, µPD63910, and µPD63911) are scheduled for availability in December 2010. Pricing for the µPD63530 SoC will be priced at US$5, and the µPD63910 and µPD63911 SoCs will be priced at US$10 each. Mass production is scheduled to begin in August 2011 and is expected to reach a combined volume of 300,000 units per month by 2012. (Pricing and availability are subject to change without notice.)

 

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power, and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.

(Remarks)

Windows Media is a registered trademark of Microsoft Corporation of the U.S.A. in the United States and other countries. All other registered trademarks or trademarks are the property of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.