Renesas Electronics Develops Package Technology that Realizes Miniaturization at the Bare Chip Level

New Technology to be Applied for Microcontrollers, Targeting Product Release in December 2011

19 Oct 2010

TOKYO, Japan, October 19, 2010 — Renesas Electronics Corporation (TSE: 6723), a premier provider of advanced semiconductor solutions, today announced the successful development of a new ultra-compact microchip package technology for use in microcontroller unit (MCU) products.

 

The newly developed technology is a kind of IC packaging technology that employs wafer-level redistribution technology, called the FO-WLP (Fan-Out Wafer-Level Package) technology, which makes it ideal for ultra-compact MCU products. It utilizes multilayer interconnect technology and chip bonding technology, two elemental technologies from Renesas Electronics' SMAFTI™ (SMArt chip connection with Feed-Through Interposer, Note 1) technology for 3-D IC (Note 2).

 

The FO-WLP production process consists of (1) formation of redistribution layer (RDL) with copper pillar bumps (CPB) on a support wafer, (2) high-speed chip-to-wafer bonding technology using chips with electroless plated pads, (3) high-productive wafer-level mold underfilling technology for approximately 10-micrometer (µm) gaps.

 

Using FO-WLP, Renesas Electronics has succeeded in packaging an 8-bit MCU with a chip size of 1.6 millimeters (mm) × 1.6 mm in a package measuring only 2.0 mm × 2.0 mm × 0.3 mm, a reduction in volume of 80 percent from the previous package size of 3.0 mm × 3.0 mm × 0.7 mm. The two-layer metal interconnects consist of polyimide and copper (Cu), the minimum wire width/space is 15 µm/10 µm, and the interlayer via size is 20 µm.

 

Test results of the chip-RDL-board electrical connections show excellent reliability in a typical condition of 1,000 −40/+125℃ temperature cycles.

 

The newly developed FO-WLP technology can be used in a new SiWLP® (System in Wafer-Level Package) that enables multiple chips, such as an MCU and an analog/RF IC chip, to be arranged side by side with high-density interconnections between them. It makes possible greater miniaturization and higher integration, allowing multiple chips to be contained in a SiWLP about the same size as a single chip.

 

With the rapid rise in awareness of energy and environmental issues in recent years, interest is focusing on more efficient use of energy through smart grids as well as environmental sensing and control technologies such as sensor networks. At the same time, sensing and feedback technologies used in patient monitoring systems and the like are becoming increasingly important in fields such as healthcare. SiWLP technology not only makes it possible to produce ultra-compact modules integrating MCUs and analog devices, it also enhances affinity with the environment by combining sensors, actuators, and communication functions needed to implement an interface with the environment or the human body.

 

Renesas Electronics views the SiWLP technology as a cornerstone in support of advancement of these fields and plans to continue promoting innovative R&D and product development moving forward.

 

Renesas Electronics announced the results of this research at the Electronics System Integration Technology Conference (ESTC 2010) held September 14-16 in Berlin, Germany.

 

(Note 1) Announced at the 56th Electronic Components and Technology Conference (ECTC 2006).

(Note 2) In contrast to an integrated circuit chip in which elements are arranged in a two-dimensional (planar) configuration, three-dimensional integrated circuit (3-D IC) technology uses stacked layer configuration with high-density interlayer connection such as microbumps and through-silicon vias (TSV) to achieve improved performance, reduced power consumption, and higher-level integration.

Pricing and Availability

Sample shipments of MCU products utilizing FO-WLP are scheduled to begin in December 2011.

 

(Remarks) SiWLP is a registered trademark or trademark of Renesas Electronics in Japan, Germany, Spain, France, U.K., Italy, U.S., China and Korea. SMAFTI is a registered trademark of Renesas Electronics in Japan, Germany, South Korea, and Taiwan. All other registered trademarks or trademarks are the property of their respective owners.

 

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power, and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.