Intersil Announces Its First Digitally Programmable Multiphase Intel(R) VR12/12.5 Compliant Controller for Server and High-End Desktop Applications

ISL6388 is highly configurable, easy-to-implement and highly integrated with best-in-class transient response

03 Jun 2014

MILPITAS, Calif., June 3, 2014 (GLOBE NEWSWIRE) -- Intersil Corporation (Nasdaq:ISIL), a leading provider of innovative power management and precision analog solutions, today announced the ISL6388, a 6-phase pulse-width modulation (PWM) controller with non-volatile memory (NVM) that is compliant with Intel's VR12/12.5 specification. Designed for server and high-end desktop applications, the ISL6388 digitally programmable multiphase controller features multiple time programmable NVM that allows for the creation of custom configurations during the design process, eliminating the need for a soldering iron to make adjustments. The new multiphase controller is supported by the company's latest release of the PowerNavigator™ graphical user interface, which allows designers to easily use Intersil's digital power products without writing a line of code. The ISL6388's patented enhanced adaptive pulse positioning (EAPP) architecture provides outstanding transient response using a linear control loop, avoiding beat frequency issues, and improving transient response over competitive solutions.

Stock Price
Investor Relations

A photo accompanying this release is available at http://www.globenewswire.com/newsroom/prs/?pkgid=25672

 

Designers today are looking for power management solutions that can exceed the power delivery requirements of modern processors, with all of the programming and monitoring capabilities of digital control. Intersil's new ISL6388 provides the best of both worlds with a fast control loop combined with full digital communication and telemetry options to enable ultimate flexibility and customization. The ISL6388 was designed to enable users to load distinct configurations into each of the eight NVM banks to optimize their power design and increase the speed of development while providing support for multiple designs in production.

 

The configurability capabilities of the ISL6388 are further enhanced by Intersil's PowerNavigator GUI, which is an easy-to-use, drag-and-drop, free downloadable interface that provides the flexibility designers need to quickly set up and control any power supply architecture. PowerNavigator's "hardware-free" mode lets users select components prior to hardware development, without design digital risk. The PowerNavigator 5.1 GUI provides access to all commands and setup configurations, including the ability to load predefined configurations for common applications. This enables unprecedented ease of use when coupled with the company's digital controller solution.

 

In the computing market, transient performance and efficiency are some of the biggest concerns for designers, especially when fast transients can result in beat frequencies. The ISL6388's advanced patented EAPP architecture utilizes a linear loop, eliminating the setup complexity of competitive solutions while providing greater bandwidth, thus improving system performance and reducing output capacitance. Combined with adjustable auto phase dropping and diode emulation, the ISL6388 can deliver high efficiency across the entire load range.

 

The ISL6388 is a highly integrated part that incorporates internal, adjustable compensation and device settings through the PMBus interface to reduce the number of external components. As a result, the ISL6388 can implement a high power 6 phase output with a minimal number of external components reducing board space and saving BOM cost.

 

"The introduction of the ISL6388 digitally programmable multiphase controller confirms Intersil's leadership position in the server and high-end desktop space by providing a fully programmable digital solution with best-in-class transient response," said Mark Downing, senior vice president of Infrastructure and Industrial Power Products at Intersil. "With the ISL6388, our customers can quickly design and configure their core power systems on the fly with the assistance of our easy to use PowerNavigator GUI to reduce costly hardware changes and speed time to market."

 

Features and Specifications

  • Intel VR12.5/VR12 compliant for core and memory
    • Programmable IMAX, TMAX, BOOT, DVID rate, address
    • SMBus/PMBus/I2C compatible
      • Up to 1.5MHz bus interface with SVID conflict free
      • NVM to store up to eight configurations with programmable frequency, droop, auto, faults (OCP, UVP, CFP)

 

  • Advanced linear EAPP control scheme
    • Digitally programmable compensation
    • Auto phase shedding option for high efficiency across load
    • Variable frequency control during load transients to reduce beat frequency oscillation
    • Linear control with evenly distributed PWM pulses for better phase current balance during load transients
    • Voltage feed-forward and ramp adjustable options
    • High frequency and PSI compensation
    • Active phase adding and dropping with diode emulation scheme for enhanced light load efficiency
    • Pb-free (RoHS Compliant) 40 Ld 5x5 Plastic Package

 

Availability

The ISL6388 is available now, priced at $3.98 (USD).

 

For more information on the ISL6388, please visit: http://www.intersil.com/products/ISL6388.

 

Intersil and the Intersil logo are trademarks or registered trademarks of Intersil Corporation. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.

 


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.