November 11, 2013

MILPITAS, Calif., Nov. 11, 2013 (GLOBE NEWSWIRE) -- Intersil Corporation (Nasdaq:ISIL), a leading provider of innovative power management and precision analog solutions, today extended its global leadership in digital power technology, introducing a major breakthrough in digital power design – the PowerNavigator™ graphical user interface (GUI). The PowerNavigator GUI lets users design digital power into their systems without writing a single line of code, and its easy-to-use drag-and-drop interface significantly accelerates design time.

A photo accompanying this release is available at http://www.globenewswire.com/newsroom/prs/?pkgid=22127

 

The PowerNavigator tool is a free, downloadable GUI that provides the flexibility designers need to quickly set up and control any power supply architecture. Crafting the power architecture in PowerNavigator's "hardware-free" mode lets users select components prior to hardware development, without design risk. The PowerNavigator GUI provides access to all commands and setup configurations, including the ability to load predefined configurations for common applications

 

Once the initial hardware is developed, the GUI can apply the saved settings and monitor all the rails. Any number of rails can be displayed with a selection of telemetric data. Designers make final system adjustments through the GUI with simple and intuitive controls. Sequencing of the rails is now possible through a visual drag-and-drop interface.

 

The rapidly expanding lineup of Intersil digital power ICs and modules provide a PMBus™ serial interface to configure, control and monitor the power supply. As part of the next generation platform, Intersil also announced today the ZL8800, a compensation free digital power controller that works in tandem with the PowerNavigator GUI to speed design time. http://www.intersil.com/ZL8800

 

For a complete look at how a designer uses Power Navigator, visit http://www.intersil.com/powernavigator

 

  • Hardware-free mode lets users design and architect power systems prior to hardware development
  • Graphical monitoring makes display easy to read with entire system on one page
  • Visual sequencing lets users sequence up and down multiple rails using drag-and-drop
  • Command line tool enables simple access and control of any PMBus command
  • Ability to save entire system project
  • Config files allow individual files to be saved for production programming
     

Intersil and the Intersil logo are trademarks or registered trademarks of Intersil Corporation. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.

 


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

Share this news on