IDT Offers Avalanche Technology’s MRAM Devices to Complement its Broad Range of Semiconductor Devices

Stock Price
Investor Relations

Collaboration allows IDT to be a single source of the primary semiconductor devices for factory and industrial automation, IoT, medical device and other growing markets.

17 Oct 2019

SAN JOSE, Calif., October 17, 2019 – Integrated Device Technology, Inc. (IDT), a wholly owned subsidiary of Renesas Electronics Corporation (TSE: 6723), today announced that it now offers Avalanche’s magnetic RAM (MRAM) devices to complement the extensive range of power, sensor, timing and microcontroller devices from Renesas. This allows IDT to serve as a single source for all the primary semiconductor devices manufacturers need for industrial control and automation systems, programmable logic controllers, medical diagnostic probes and equipment, multifunction printers, and IoT devices.

Avalanche’s MRAM devices are ideal for high-speed, non-volatile memory applications such as program storage and data backup. IDT will offer Avalanche’s 4Mbit, 8Mbit and 16Mbit MRAM devices in two packages (SOIC and WSON) with two different temperature ratings (85°C and 105°C). Available speeds will be up to 108MHz, with configurable interfaces for SPI, DPI, QPI with Single-Data-Rate and Double-Data-Rate modes.

“We are excited by this collaboration with Avalanche Technology, as we can now offer our customers the widest range of serial interface MRAM products,” said Steven Lee, technical director of the IoT sensors group at IDT. “Avalanche’s MRAM devices are an ideal complement to our own industry-leading lines of power, sensor, timing and microcontroller devices.”

“Avalanche is bringing added benefit to our customers by enabling new usage models in industrial and automotive designs where data integrity and reliability, as well as persistence, are key,” said Danny Sabour, VP of Marketing and Business Development of Avalanche technology. “Teaming up with IDT, a world leader in semiconductor manufacturing, enables us to bring our leading edge products to market more quickly.”

 

About Avalanche Technology

Avalanche Technology Inc. is the leader in next generation Perpendicular STT-MRAM technology. Avalanche is accepted as the front-runner to replace traditional Flash and SRAM for unified memory architectures in future SOC systems, and delivers high performance and low power at 55, 40 and 28nm with scalability to 22 and 14nm. With a proven STT-MRAM portfolio at multiple geometry nodes, combined with an intellectual property portfolio of over 300 patents and applications, Avalanche Technology is delivering on the promise of enabling the next generation of scalable embedded unified memory architecture for use in GPUs, MCUs, DSPs, ASSPs and ASICs, making it the true “Next Generation MRAM Company.” For more information, visit us online at www.avalanche-technology.com.

 

About IDT

Integrated Device Technology, Inc., a wholly owned subsidiary of Renesas Electronics Corporation (TSE: 6723), develops system-level solutions that optimize its customers’ applications. IDT’s market-leading products in RF, high performance timing, memory interface, real-time interconnect, optical interconnect, wireless power and smart sensors are among the company’s broad array of complete mixed-signal solutions for the communications, computing, consumer, automotive and industrial segments. Headquartered in San Jose, Calif., IDT has design, manufacturing, sales facilities and distribution partners throughout the world. Additional information about IDT can be found at www.IDT.com. Follow us on Facebook, LinkedIn, Twitter, and YouTube.

 

©2019, Integrated Device Technology, Inc. IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc., and its worldwide subsidiaries. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.