IDT Wins Prestigious ACE Award for VersaClock 5 Programmable Clock Generator

Stock Price
Investor Relations

Introduced in 2014, the VersaClock 5 Timing Device Features Best-in-Class Performance at Half the Power of Competing Devices

22 Jul 2015

SAN JOSE, Calif., July 22, 2015—Integrated Device Technology, Inc. (IDT®) (NASDAQ: IDTI) today announced it won an ACE Award for its innovative VersaClock® 5 programmable clock generator. The award was presented Tuesday by EE Times and EDN, two prestigious industry publications, at the annual ACE Awards ceremony.

A panel of technology experts selected the VersaClock 5 device as an “Ultimate Product” in the Logic/Interface/Memory category.

“We thank the judges for this recognition of some truly innovative technology,” said Dave Shepard, vice president and general manager of IDT’s timing and RF division. “This ACE Award is further validation of the value the VersaClock 5 technology has brought to the market.”

Featuring best-in-class jitter performance at half the power of competing devices, IDT’s multi-output VersaClock 5 timing solution consolidates system components with superior design flexibility, making it ideal for cost-sensitive, low-power consumer and low-jitter communications applications. In addition to the VersaClock 5 nomination, IDT was a finalist for Company of the Year, Executive of the Year (CEO Greg Waters), and the STEM Impact Award.

 

About IDT Clock and Timing Solutions

With a product portfolio 10 times greater and broader than any other, IDT is the world’s leader in silicon timing and is in a unique position to address the needs of virtually any application. With the industry’s largest market share, IDT is the only one-stop-shop for timing, offering products from full-featured system solutions to simple clock building-block devices. Factory-programmable options and clock solution customization capabilities address unique customer requirements, while the lowest jitter and lowest power features set IDT apart from the competition. Products are accompanied by a world-class support team driven by service and responsiveness goals. For more information about IDT’s leading portfolio of timing products, please visit http://www.idt.com/go/timing.

 

IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.