IDT, NVIDIA and Orange Silicon Valley Drive Supercomputing to Edge of Wireless Network for Real-Time Analysis and Services

Stock Price
Investor Relations

New Platform’s Mobile GPU Clustering Enables Big Data Analytics at Local Base Stations for More Timely and Pertinent Results

25 Feb 2015

SAN JOSE, Calif., Feb. 25, 2015-- Integrated Device Technology, Inc. (IDT®) (NASDAQ: IDTI) announced today that it has developed with NVIDIA® and Orange Silicon Valley a supercomputing platform that can analyze 4G to 5G base station bandwidth data in real time, enabling network operators to monetize the voluminous data flowing through their communications systems. By connecting clusters of low-power NVIDIA Tegra® K1 mobile processors with IDT’s RapidIO interconnect and timing technology, the platform can deliver real-time data that network operators can use to provide consumers a more responsive and interactive experience.

Designed for high-performance computing, IoT appliances and wireless access networks handling 4G and higher traffic, the platform features cutting-edge deep learning and pattern recognition computing capabilities. By installing the hardware at multiple, geographically dispersed base stations along the edge of the network, the Big Data problem is solved by distributing the computing capacity and delivering lightning-quick analysis of locally generated data, such as social media content.

“For example, if you tweet that you’ve just seen a movie and are headed out to dinner, some nearby dining options could pop up on your screen,” said Sailesh Chittipeddi, IDT’s vice president of Global Operations and chief technology officer. “Or the technology can be used for mass transit; if you’re standing at a bus stop, you can check your phone for the precise location of your bus. The possibilities are virtually endless.”

Chittipeddi refers to the platform as “supercomputing at the edge” because the technology is deployed and analysis conducted at local base stations—at the edge of the wireless network—rather than in a central location, removing the bottleneck between the base station and the core of the network. “The solution was developed with an architecture designed to handle the emerging market for geographically distributed analytics, deep learning and pattern recognition in real time,” he said.

"By taking mobile low-power GPU technology and connecting it with 100 ns latency RapidIO interconnect, this modular cluster can be deployed to distribute high-performance compute functionality to the edge of the wireless network, where it is most geographically sensitive," said Jag Bolaria of the Linley Group. "The innovation paves the path for co-locating real-time deployable analytics in the approximately 2 million base stations deployed annually in wireless networks."

The Supercomputing at the Edge platform uses IDT’s 20 Gbps interconnect technology to connect a low-latency cluster of NVIDIA Tegra K1 mobile processors. It’s suitable for micro base station deployment along with larger computing clusters in the C-RAN, a new cellular network architecture. Each computing card is based on connecting up to 4 GPU units per processing card connected with RapidIO low-latency NIC and switching products on board.

The platform, which can support up to 12 teraflops per IU RapidIO server blade, is based on servers from Prodrive Technologies (www.prodrive-technologies.com) and computing cards from Concurrent Technologies PLC (www.gocct.com). Each computing card contains four NVIDIA mobile processors. The processors deliver 192 fully programmable CUDA cores for advanced graphics and compute performance. Each card in the system matches computing cores with 20 Gbps interconnect to each GPU, with over 140 Gbps of built-in switching at each node with IDT’s best-in-class timing solutions

IDT will present the Supercomputing at the Edge platform at the Linley Data Center Conference Feb. 25-26 in Santa Clara, Calif., and Mobile World Congress March 2-5 in Barcelona, Booth 1H10.

 

IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. NVIDIA® (NASDAQ: NVDA) is a registered trademark of NVIDIA Corporation in the United States and other countries. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.