FAQ Search Results No. 106091
FAQ 106091
Latest Updated:10/29/2007
Functions: ;
Can 32185/32186 and 32192/32195/32196 Groups be debugged using an emulator
that does not support the SDI-3 specification?
Emulators that do not support SDI-3 specification (compatible debugger:
M3T-PD32R)
- M32170T-SDI
- M32100T-SDI-E
- M32100T2-SDI-E
If you are not using the trace function or the time measurement function,
you will have no problems debugging the 32185/32186 and 32192/32195/32196
Groups.
If you are using the trace or time measurement functions, the following
restrictions apply.
[Usage Restrictions]
Compared to results gained when using an SDI-3 specification compatible
emulator, use of an emulator that does not support SDI-3 will cause an increase
in lost trace data, resulting in the following phenomena.
| (1) | Increased loss of trace results. | |
| (2) | Increased occurrences of trace events failing to occur. | |
| (3) | Increased occurrences of H/W breaks failing to occur. A H/W break is generated when the emulator detects break conditions based on the trace results. Increases in lost trace data will result in fewer H/W breaks generated. The PC break, chip break and S/W break can be used normally. |
|
| (4) | Increased occurrences of time measurement events failing to occur. |
When you need to use the trace function or time measurement event, we recommend
using the following new emulators, which support the SDI-3 specification.
Emulators supporting SDI-3 specification (corresponding
debugger:M3T-PD32RM)
- M32100T3-SDI-E
- M32100T5-SDI-E
The MCU files for the 32185/32186 and 32195/32196 Groups are available at FAQ 106090.
Was this information useful to you? Yes NO
Suitable Products| 32185 |
| 32186 |
| 32192 |
| 32195 |
| 32196 |
| M32100T2-SDI-E |
| M32100T-SDI-E |
Japan English