Stub Generator
The following page content corresponds to the products marketed in Japan.
If you do not live in Japan, please
- Overview
- Design Support
- Further Information
Compatible Real-Time OS
Overview
The stub generator is a tool to generate client and server stub source code
that is needed when using the RPC (Remote Procedure Call) functions of the
HI7200/MP.
By creating a Config file for the stub generator using a text editor and
putting it into the stub generator, it is possible to generate the C source
code for the client and server stub. The stub generator is executed as a Perl
script. The Perl runtime environment needs to be prepared by the user.

Japan English