The following page content corresponds to the products marketed in Japan.
If you do not live in Japan, please
- Overview
- Documentation
- Downloads
- Design Support
- Further Information
- About Agreement
- Alliance Partners
For real-time OS products, a software licensing agreement must be entered upon purchase of a mass-production license. However, since shrink wrap agreements are used for evaluation licenses, you have only to agree to the contents of the agreement when you unseal the product, and a formal software licensing agreement is not required. Agreement types and distribution are as described below.
For agreement details, contact your nearest sales office or representative.
Real-time OS product agreement format for SuperH/V850/RX/RL78/78K0R/R8C/M16C/H8SX/H8S
(Applicable for the following Real-time OS;
HI7300/PX, HI7750/4, HI7700/4, HI7200/MP, HI7000/4, RI850V4, RI600V4, RI600/4, RI600/PX, RI78V4, MR8C/4, M3T-MR100/4,
M3T-MR308/4, M3T-MR30/4, HI1000/4)
OS Agreement Details
| Agreement Type | Mass-production License | Evaluation License | ||
|---|---|---|---|---|
| With source code | No source code | No source code (Shrink wrap agreement) | ||
| Product Deliverables | OS Source Code | Yes | No | No |
| OS Object Code | Yes | Yes | Yes | |
| Sample Source Code | Yes | Yes | Yes | |
| Manual | Yes | Yes | Yes | |
| License Grant | Right for Internal Use | Yes | Yes | Yes |
| Right to Reproduce | Yes (Unlimited) | Yes (Unlimited or 3,000)* | Yes (Internal use only, unlimited copies) | |
| Right to Modify Program | Yes | No | No | |
| Host Machine Limitation | Unlimited | Unlimited | Limited number of hosts (1 or Unlimited)** | |
| Application Limitation | Limited | Limited | Unlimited | |
| Device Limitation | Limited | Limited | Unlimited | |
Explanation of terms:
Yes: Included in the license. No: NOT included in the license.
*. For "right to reproduce" of the MR8C/4 mass-production license (no source code) , only "Unlimited" can be chosen.
**. For "host machine limitation" of the MR8C/4 evaluation license, only "1" can be chosen.
- Note:
- License grants are valid until the Licensee informs Renesas of the relinquishment of rights. All licenses are for use only, and do not grant property rights.
Explanation of Terminology Used in the OS Agreement
| Mass-production License | This license permits the Licensee to market or sell a product which incorporates the real-time OS. The mass-production license also permits prototype development. Separate purchase of an evaluation license is not necessary for development. |
|---|---|
| Evaluation License | This license permits the Licensee to install the software on up to a designated number of host machines, and use in prototype development. There is no limit to the number of prototypes with built-in real-time OS which may be developed; however, the license is restricted to application in prototype development only. |
| Right for Internal Use | The Licensee can use the real-time OS object code internally (within the Licensee's department, etc.) on supported MCUs. This right assumes that the real-time OS is used only in a prototype system for development. |
| Right to Reproduce | The Licensee can use the real-time OS object code on multiple devices. For the mass-production license, the maximum number of reproductions must be entered in the agreement. The Licensee can choose to set the number of reproductions as either unlimited or 3000 (agreements which include source code must be unlimited). The price varies according to the number of reproductions. |
| Host Machine Limitation | The real-time OS is provided on media such as a CD. The Mass-production license limits the number of host machines on which the contents of this media may be installed (choice between 1 or Unlimited). |
| Application Limitation | For the mass-production license, the basic name of the Licensee's application (or project) must be written in the agreement. (For example, ink-jet printer, color copy machine for professional use, economy car navigation system, etc.) A new agreement is required if the application changes. |
| Device Limitation | The MCU type on which the OS is to be incorporated must be written in the agreement. A new agreement is required if the target MCU changes. |
Ordering Information
| Product Type | Part Number |
|---|---|
| HI7200/MP | R0R50720MRW01w |
| HI7300/PX | R0R50730PRW01w |
| HI7750/4 | R0R40775TRW02w |
| HI7700/4 | R0R40770TRW02w |
| HI7000/4 | R0R40700TRW02w |
| RI850V4 | R0R08500TCW01w |
| RI600V4 | R0R5RX00TCW01w |
| RI600/4 | R0R5RX00TRW01w |
| RI600/PX | R0R5RX00PRW01w |
| RI78V4 | R0R07800TCW01w |
| M3T-MR100/4 | R0R56400TRW01wE |
| M3T-MR308/4 | R0R30800TRW02wE* |
| M3T-MR30/4 | R0R30600TRW02wE |
| MR8C/4 | R0R52100TRW01wE |
| HI1000/4 | R0R41600TXW01w |
- *. M3T-MR308/4 with this part number does not support DVP-M2(S) nor DVP-C3. If you need an M3T-MR308/4 which supports DVP-M2(S) or DVP-C3, please contact your nearest Renesas Electronics sales office or distributor.
NOTE:
The lower-case 'w' in the part number denotes the type of license. Replace with the numeral or letter from the following table according to the type of license you want. For example, In mass-production license for RI78V4 for manufacturing the unlimited number of products with the source code closed, the Part Number is R0R07800TCW01U.
| 1 | Evaluation license; Can be installed on only one host machine. |
|---|---|
| A | Evaluation license; Can be installed on an unlimited number of host machines. |
| K | Mass-production license; Can be embedded in up to 3000 products; the source code is not disclosed. |
| U | Mass-production license; Can be embedded in an unlimited number of products; the source code is not disclosed. |
| Z | Mass-production license; Can be embedded in an unlimited number of products; the source code is provided. |
RX850V4 and RX78K0R Real-time OS product agreement format for V850/78K0R
For the detailed information about Real-time OS product agreement format for RX850V4 and RX78K0R, please contact your nearest sales office or representative.
Japan English