The following page content corresponds to the products marketed in Japan.
If you do not live in Japan, please
- Overview
- Documentation
- Design Support
- Further Information
- Where is OSEK/VDX required?
- Why is OSEK/VDX required?
OSEK/VDX can be used for various applications. It is suitable for applications, such as the automotive field, the construction apparatus field, FA field, etc. which especially uses CAN.
Application field: In the case of an automobile LAN system(Example)

Japan English