Skip to main content

The following page content corresponds to the products marketed in Japan.
If you do not live in Japan, please

  • Conditions of Use

Conditions of Use

[Compiler Packages]

If you use the following version of the compiler packages, the added CPUs in the Device File Updater can be selected from the "CPU Type" list when you are creating a new project workspace.

  • C/C++ Compiler Package for SuperH Family V.9.00 Release 00 or later *
  • C/C++ Compiler Package for RX Family V.1.00 Release 00 or later
  • C Compiler Package for R32C Series V.1.01 Release 00 or later
  • C Compiler Package for M16C Series and R8C Family [M3T-NC30WA] V.5.42 Release 00 or later **
  • C/C++ Compiler Package for H8SX, H8S, H8 Family V.6.02 Release 00 or later

    * If the C/C++ Compiler Package for SuperH Family V.9.03 Release 02 or later has not been installed in your PC, the Device File Updater cannot be downloaded. It is required that you install the latest compiler package in advance to download the Device File Updater. Even if the latest version of the compiler package is installed, the previous version is not deleted, so you can use the latest and the previous versions of it in High-performance Embedded Workshop. When downloading the Device File Updater under this environment, the added CPUs in the Device File Updater can be selected in all versions of the C/C++ Compiler Package for SuperH Family V.9.00 Release 00 or later.

    ** If the C Compiler Package for M16C Series and R8C Family [M3T-NC30WA] V.5.45 Release 00 or later has not been installed in your PC, the Device File Updater cannot be downloaded. It is required that you install the latest compiler package in advance to download the Device File Updater. Even if the latest version of the compiler package is installed, the previous version is not deleted, so you can use the latest and the previous versions of it in High-performance Embedded Workshop. When downloading the Device File Updater under this environment, the added CPUs in the Device File Updater can be selected in all versions of the C Compiler Package for M16C Series and R8C Family [M3T-NC30WA] V.5.42 Release 00 or later.

[Integrated Development Environment (IDE)]

Related Resources


End of content

Back To Top