Skip to main content

The following page content corresponds to the products marketed in Japan.
If you do not live in Japan, please

User Interface Options

The Flash Development Toolkit has three user-friendly GUIs which are available to choose the one depending on the purpose of use.

[With generating project]

There are two types of choosable windows as follows: the main window that provides various useful functions, and the simple interface window that is a simplified version of the main window.

  • Main window
    Thanks to its project management function, this window permits data management for a system comprised of multiple microcomputers and data management in each development phase to be exercised efficiently. Furthermore, its data editing function permits you to edit parameters easily.
    This window provides you the convenient environment during a development stage.

  • Simple interface window
    You can use this window by calling it from the main window after creating a project. By using the project management function, you can write data for multiple projects to your MCU easily.
    This window provides you the convenient environment when it is used during a mass-production stage or when there are multiple data and devices to manage.

 

[Without generating project]

Basic window is a simplified version of the main window.

  • Basic window
    You can use this window by starting it directly. This window permits you to write data to your MCU easily without having to create a project. This window provides you the convenient environment when used during a mass-production stage or when there are one data and device to manage.
    Note: This window is available from Ver.3.

 

Related Resources


End of content

Back To Top