Skip to main content

The following page content corresponds to the products marketed in Japan.
If you do not live in Japan, please

Target Devices

  • AE-5 Series

Overview

E6000H emulator is a tool to support system development targeted at Renesas microcomputers in aspects software and hardware.
E6000H emulator can be used for application software development and debugging on its lone , and also used for debugging of the user system as connected to the user system via an user system interface cable.
The HS0AE5EPH60H is an SE-I emulator with USB I/F for 32-bit smart card microcontroller, AE-5 Series.

Target devices and options

(As of Oct. 01, 2010)

Target devices
PC Interface
(User-selectable)
User interface cable
or
User cable
Series
Type name
AE-5
(32 bit)
AE55C1
AE58C
AE57C1
AE57C

HS6000EIU02H
(USB-Adapter)

HS6000EIP02H *1
(PC-Card)
(Discontinued)

HS6000EIC02H}
(PCI-Card)
(Discontinued)

HS6000ELN01H
(LAN-Adapter)
(Discontinued)

Included in the package

*1. HS6000EIP01H is also available.

Related Resources


End of content

Back To Top