Skip to main content

The following page content corresponds to the products marketed in Japan.
If you do not live in Japan, please

Target Devices

  • 740 Family 38000 Series 38D5 Group

Overview

The M38D59T-RLFS is an emulator MCU board that is used by connecting to the compact emulator M38000T2-CPE or the PC4701 emulator system. It is for the 38000 Series 38D5 Group.

Components

  • Emulator MCU board (M38D59T-RLFS)
  • Evaluation MCU (M38D59RLFP) * Already mounted
  • Converter board for connecting to 80-pin 0.8mm-pitch LCC (M3T-F160-80LCC)
  • M38D59T-RLFS User's manual

Specifications

Applicable emulator Compact emulator M38000T2-CPE
or
PC4701(+M38000TL2-FPD)
Supported MCU 38000 Series 38D5 Group
Maximum operating clock frequency 12.5 MHz (in frequency/2 mode)
* It must be within the limits defined by the specification of MCU.
MCU mode Single-chip mode
Target system voltage 1.8 to 5.5[V]
Power supply Supplied from the user system

Connection Procedure

(1) Mount an LCC socket on the user system.
(2) Attach the M3T-F160-80LCC to the M38D59T-RLFS. (factory-installed)
(3) Attach the tip of the probe of the emulator to the M38D59T-RLFS.
(4) Attach the M3T-F160-80LCC to the LCC socket.

* Before using the M38D59T-RLFS, be sure to read the user's manual.

Connecting to the User System

.

Related Resources

Tool News

Try before you buy!
Evaluation Software Downloads


End of content

Back To Top