MISRA C Rule Checker SQMlint
The following page content corresponds to the products marketed in Japan.
If you do not live in Japan, please
- Overview
- Documentation
- Downloads
- Design Support
- Further Information
Functions
- MISRA C rule inspection during compilation
Source codes can be inspected against MISRA C rules by only specifying options when compiling the source files. There is no need to build an inspection-purpose environment.
- Adaptable to special options of the Renesas C compiler
If special options such as one that handles the double type as float type are used, C source codes are inspected by taking the effects of those options into consideration.
- Usable in the Renesas integrated development environments,
High-performance Embedded Workshop and TM
You can make a tag jump in Renesas integrated development environment HEW or TM based on the output results and correct the C source codes on the spot. Therefore, deviations from MISRA C rules can be corrected in the same way as when correcting compile errors.
- Inspection results output in CSV format (Report file)
The inspection results are output as report files in CSV format usable in spreadsheet software, and can be analyzed more efficiently by using bundled utilities.
Japan English