Skip to main content

The following page content corresponds to the products marketed in Japan.
If you do not live in Japan, please

Target device

  • D6X

 

Overview

AS6133

Assemblers can be classified into absolute assemblers and relocatable assemblers. The AS6133 can be classified as an absolute assembler, but it differs from conventional absolute assemblers as it allows split programming. Therefore, while you could say that AS6133 is an absolute assembler, it also has characteristics very close to those of a relocatable assembler.

 

Features

  • Can create sequence files
  • Create source module files
  • Japanese can be used
  • External module definition reference function

Related Resources


End of content

Back To Top