Skip to main content

The following page content corresponds to the products marketed in Japan.
If you do not live in Japan, please

Target device

  • 17K

 

Overview

RA17K

The RA17K is an assembler package for 17K microcontrollers. This assembler package converts programs written in mnemonics to object code which can be executed by the microcontroller. Absolute addresses are not resolved when the program is assembled, relative addresses are resolved in section units. PM integrates RA17K and SIMPLEHOST and provides a development environment on Windows. In this way, program development can be efficiently done in simple operations. The RA17K has an absolute mode which has almost the same function as an absolute assembler (AS17K: previous product). The following programs are included with the RA17K. PM, Assembler (RA17K), Linker (LK17K), Make (MAKE), Sequence file converter (CNV17K), Document processor (DOC17K), idea-L Light editor

 

Features

  • Relocatable assembler for the 17K
  • Includes utilities such as a linker, make, and a document processor
  • Source programs can be written in Japanese
  • Has embedded macro instructions
  • Document creation function
  • AS17K compatibility mode (absolute mode)

Related Resources


End of content

Back To Top