| FAQs |
-
FAQ NO : 1000485
Issue Date : Jun.28.11
- Functions : General MPU/MCU
- How can I write programs in the flash memory connected to SuperH MCU?
- You have two options as described below.1. Writing programs with an emulator with the function that supports writing to an external flash memory. Please check the specification of your emulator.When you use Renesas Electronics E10A-USB emulator, pleas...
Relevant Products
- SH7730
- SH7723
- SH7722
- SH7760
- SH7751R
- SH7751
- SH7750S
- SH7750R
- SH7729R
- SH7727
- SH7721
- SH7720
- SH7709S
- SH7706
- SH7705
- SH7286
- SH7285
- SH7263
- SH7261
- SH7243
- SH7211
- SH7206
- SH7203
- SH7201
- SH7146, SH7149
- SH7131, SH7132, SH7136, SH7137
- SH7083, SH7084, SH7085, SH7086
|
|
-
FAQ NO : 102181
Issue Date : Mar.25.09
- Functions : Bus State Controller/External Bus Interface
- Is it possible to switch between little Endian and big Endian?
- Yes, it is possible to switch between little endian and big endian by designating an MD5 pin. At the time of a power-on reset, big endian is engaged when MD5 is low; little endian is engaged when MD5 is high. This designation is effective for the...
|
-
FAQ NO : 102791
Issue Date : Mar.25.09
- Functions : Cache Memory
- What is coherency ?
- Coherency means that data is matched between cache and external memory. For example, writing to external RAM is not performed if the cache is hit when the cache is used in write back mode. Unmatching of data between the cache and external RAM o...
|
-
FAQ NO : 102796
Issue Date : Mar.25.09
- Functions : Cache Memory
- Is it possible to turn the cache OFF in the specific address space?
- Please use P2 area when using with cache OFF because cache is disabled in P2 area within the address spaces of SH-3 and SH3-DSP, and use P0 area when using with cache ON because cache is enabled in P0 area.
|
|
-
FAQ NO : 105335
Issue Date : Mar.25.09
- Functions : Subclock
- Is there any note when RTC is not used?
- When RTC is not used, the standby mode (software standby mode) cannot be canceled by IRQ, IRL, PINT and each interrupt of on-chip peripheral functions. Cancel the standby mode (software standby mode) by NMI or reset when RTC is not used. ...
|
|
-
FAQ NO : 105661
Issue Date : Mar.25.09
- Functions : Bus State Controller/External Bus Interface
- What should be confirmed when it cannot access SDRAM?
- Please confirm the following. 1. Please confirm the clock ratio of internal clock (IΦ) and bus clock (BΦ) should NOT be IΦ:BΦ=1:1 In SH7709S/SH7729R/SH7706/SH7727, it is NOT possible to access SDRAM when it is IΦ:BΦ=1:1 (In SH7705/SH772...
|
|