There are a full-spec emulator (E100) and two on-chip debugging emulators (E1 and E20) available for the RX610 Group. E1 Emulator  This is an on-chip debugging emulator, and the user connects it to the MCU mounted on the user’s substrate. Usability is similar to that of the E10A-USB, which was popular with the SH family products” and the E8a emulator widely adopted with the R8C family products. The emulator supports performance measurement function in addition to the basic debugging functions such as program download, step execution, and break. As the debugging is performed using the actual chip on the user’s substrate, it is suitable for evaluating the A/D, D/A, and other analog functions. The emulator may also be used as an on-board flash programmer for flash programming of the RX, and act as a power supplier of up to 200mA. In case of the RX600 Series, the emulator is connected to the user system via a 14-pin connector, and to a PC via USB. It is so “low-cost and compact” that it is realistic for each member of a development team to have one emulator. E20 Emulator  This is an on-chip debugging emulator, and the user should connect it to the MCU mounted on the user´s substrate. The functions and usability are similar to the E10A-USB that was popular with the SH family products. In addition to the E1 Emulator’s basic debugging functions, the E20 offers more advanced debugging capabilities, such as large-capacity tracing to check the execution history, and real-time RAM monitoring to monitor the changes in data during execution of a program. E100 Emulator (Scheduled to be supported for RX)  The E100 emulator has full bus trace and is available for in-circuit emulation in system designed around the various Renesas MCU Platform of processors. It enables full-bus tracing of the RX600 Series products using the rich functions including real-time profiling. It has the performance sufficient for debugging any software for the RX, with the maximum operating frequency of 133MHz, trace capacity of 4M cycles, 4096 software break points and hardware break points up to 16. When using on the RX, the user should connect an MCU unit for the RX (under development) and use a dedicated connection socket. |