Skip to main content

The following page content corresponds to the products marketed in Japan.
If you do not live in Japan, please

Overview

The H8/300H CPU is a high-speed central processing unit with an internal 32-bit architecture that is upwards-compatible with the H8/300 CPU. The H8/300H CPU has sixteen 16-bit general registers, can address a 16-Mbyte linear address space, and is ideal for real-time control.

Examples of main applications

  • Consumer: White goods (refrigerators, washers, dryers, cooking ranges, etc.), appliances (vacuum cleaners, etc.), game pads, home electronics
  • Industrial: HVAC system, thermostats, controllers for small DC brushless motors, stepper motors
  • Office Automation: Mechanical control for fax machines, printers, measurement devices
  • Automotive: Control systems for power windows, windshield wiper controls, keyless entry systems, side airbags

 

Lineup:

H8/36109

The H8/36109 Group is a high-end product in the H8/36049 Group that is suitable for motor control, and the highest performance product in the H8/Tiny Series.
This group offers increased ROM and RAM, and enhanced peripheral functions such as a 5-channel a 16-bit timer and 16-channel A/D converter. In addition, there liability of the fail safe functions is improved by incorporating anon-chip oscillator.

H8/36077, H8/36079

The H8/36077 Group offers enhanced fail safe functions (oscillation stop detection function: the watchdog timer starts operating after the reset state is canceled) based on the H8/3687 Group. Peripheral functions match those of the H8/3687 Group, including a 16-bit timer with two channels, a two-channel asynchronous/synchronous serial interface, and a one-channel I²C bus interface. This group can be used for to motor control thanks to the added 2-channel 16-bit timer. Moreover, it can also be used for network-connected home appliances by employing the two-channel serial communication interface and one-channel I²C bus interface.

H8/36087

The H8/36087 Group provides high-speed operation (18 MHz) at 3 V and is based on the H8/3687.

H8/36064

The H8/36064 Group is a slim version of the H8/3687. The device has 32 kbytes on-chip single supply flash memory.

H8/36049

The H8/36049 Group is a version of the existing H8/3687 Group, but with enhanced peripheral functions and I/O, and is suitable for use in household appliances with advanced functions, including indoor units of air conditioners needing motor control, etc.

H8/36037, H8/36057

The H8/36037 and H8/36057 Groups have an on-chip CAN (full CAN 2.0B) interface for use in in-vehicle equipment such as door modules and airbags.

H8/36014, H8/36024

The H8/36014 and H8/36024 Groups offer the high-speed H8/300H Tiny CPU core with enhanced communication functions based on the H8/3672 Group and are optimized to provide low-cost solutions for small communications networks in applications such as fire and security systems.

H8/36912, H8/36902

The H8/36912 and H8/36902 Groups are microcomputers with the lowest-capacity(8 kbytes) and lowest pin count (32 pins) in the H8/300H Tiny lineup. With enhanced timers, 10-bit A/D converter, asynchronous/synchronous serial interface, I2C bus interface (H8/36912 only) and large- current ports, these devices are suitable for applications including system control for small home appliances and various sensors.

H8/36094

The H8/36094 Group offers enhancement of fail safe functions (Oscillation stop detection function, the watchdog timer starts operating at initial value.) based on the H8/3694 Group. H8/36094 Group can be used for various purposes from main microcomputer at small system to sub microcomputer at large system because peripheral functions as H8/3694 Group include timer of four types, I2C Bus Interface, Serial Communication Interface, 10 bit A/D converter.

H8/3694

The H8/3694 Group is the successor to the H8/3664 Group. The maximum frequency has been increased to 20 MHz at 5 V power supply, and operability is highly enhanced by improvement of the I2C1 interface. Four types of packages are available: a 64-pin LQFP (10 mm x 10 mm) and 64-pin QFP (14 mm x 14 mm) having pin compatibility with the H8/3664 Group, plus two 48-pin LQFPs (10 mm x 10 mm and 7 mm x 7 mm) which are newly introduced as part of this group.

H8/3687

The H8/3687 Group offers enhancement of the peripheral functions of the H8/3664 and is optimized to achieve higher performance.

H8/3672

The H8/3672 Group was developed for smaller, cost sensitive applications which don't require all of the functions of the H8/3664.

H8/3664

This group is supported only for the customers who have already adopted any of the products. For new adoption, please consider H8/3694 Group, H8/36094 Group products.


End of content

Back To Top