Skip to main content

The following page content corresponds to the products marketed in Japan.
If you do not live in Japan, please

Overview:

H8/300H MCUs deals efficiently with high volumes of data with a embedded 512KB Flash microcomputer. High compatibility with the H8/300 all allow greater efficiency, making it an ideal command system. H8/300H family of microcontrollers are 16-bit MCUs integrated around original Renesas H8/300H CPU core.

 

This series is supported only for the customers who have already adopted any of the products.
For new adoption, please consider H8S Family or H8SX Family products.

Roadmap:


End of content

Back To Top