Skip to main content

Renesas Electronics Introduces Three New Power MOSFET Products that Realize High-Efficiency DC/DC Converters for Servers and Notebook PCs

Product Specifications of the 12th-Generation Power MOSFET Products

Ta = 25℃

Product Max. Rating On-Resistance (RDS (on)) (mΩ) Qg (nC) Qgd(nC)
VDSS(V) VGSS(V) ID(A) VGS = 4.5 V VGS = 10 V
typ. max. Typ. max.
RJK0210DPA 25 +16/−12 40 5.7 7.4 4.5 5.4 11.8 1.2
RJK0211DPA 25 +16/−12 30 8.7 11.3 6.8 8.2 7.5 0.9
RJK0212DPA 25 +16/−12 25 12.0 15.6 9.0 10.8 5.4 0.6
  • Reference Diagram

Comparison of voltage conversion efficiency between a voltage conversion circuit in which the new RJK0210DPA was used for control and one in which the RJK0365DPA-02 10th generation power MOSFET was used. (In both cases the RJK0208DPA was used as the synchronous rectifier power MOSFET.)

RJK0210DPA (12th generation) was found to have higher voltage conversion efficiency than RJK0365DPA-02 (10th generation) at Vin = 12 V, Vo = 1.05 V, fsw = 300 kHz, 2-phase; Lo-side common: RJK0208DPA

The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

Investor Relations
Stock Price

End of content

Back To Top