Skip to main content

Renesas Electronics Introduces Two New DTV and Set-top Box SoCs for Digital TV Broadcasting Markets in Japan and South America

Aims to Expand Sales in the South American Market to 10 Billion Yen in 2013

TOKYO, July 16, 2010-- Renesas Electronics Corporation (TSE: 6723), a premier supplier of advanced semiconductor solutions, today announced the availability of two new system-on-chips (SoCs) for digital televisions (DTVs) and set-top boxes (STBs), the EMMA™3TJ and EMMA3TS, specifically targeting the terrestrial digital broadcasting market in Japan and South American countries such as Brazil, Argentina and Venezuela.

The EMMA3TJ SoC is intended for use in DTVs, and the EMMA3TS SoC is targeted for STBs. Both devices integrate on a single chip the functions needed to receive digital broadcasts, including (1) demodulator circuits for the ISDB-T terrestrial digital broadcast format used in Japan and South America, and circuits for the ISDB-S satellite broadcast format used in Japan, (2) decoder circuits for the MPEG2 and H.264 video compression standards, and (3) peripheral interface circuits, such as USB 2.0 and Ethernet. These key features make it easy for system manufacturers to build TVs and STBs with support for digital broadcasts. The EMMA3TJ SoC also includes functions needed to implement three-dimensional (3D) TVs, making it possible to display 3D video from digital broadcasts or Blu-ray™ discs.

Several terrestrial digital broadcast formats are currently in use, including ATSC in North America and DVB-T in Europe. The ISDB-T format used in Japan has recently been adopted by several South American countries, including Brazil, Argentina, and Venezuela. The present scale of this market is estimated to exceed 100 million TV receivers. The new SoCs were designed specifically for Japan and South America, utilizing Renesas Electronics' accumulated technology expertise, to enable reception and display of content broadcast in the ISDB-T and ISDB-S formats.

Main features of the new products:

  • (1) On-chip demodulator circuits for ISDB-T and ISDB-S

    The new SoC devices both integrate an on-chip demodulator circuit for the ISDB-T terrestrial digital broadcast format used in South American countries such as Brazil and Argentina in addition to Japan. They also have an on-chip demodulator circuit for the ISDB-S format used for BS/CS broadcasts in Japan. This makes it easy for system manufacturers to build TVs and STBs with support for the ISDB-T and ISDB-S formats.
  • (2) Support for MPEG2 and H.264

    Renesas Electronics' new SoC devices also integrate a single-chip decoder circuit supporting the MPEG2 video compression standard, used for terrestrial digital broadcasts in Japan, as well as the H.264 standard, that provides twice the compression and is expected to be widely adopted worldwide, including in Europe and South America. This feature provides the capability to decompress and display compressed video data using either of the above standards.
  • (3) On-chip external interface functions for USB 2.0 and Ethernet

    The new SoC devices include the built-in USB2.0 interface and Ethernet MAC (media access controller), which enable display of video content delivered via the Internet, including video on demand and streaming broadcasts.
  • (4) Software compatibility

    The same architecture is used for the EMMA3TJ and EMMA3TS SoCs, assuring software compatibility, which provides flexibility and easing development of software applications.
  • (5) Ability to display 3D video data (EMMA3TJ SoC only)

    The EMMA3TJ SoC integrates essential functions for developing 3D TVs including a decoding circuit for input signals in the 3D format specified by the HDMI1.4a standard. This makes it possible to build TVs capable of displaying 3D video from digital broadcasts or Blue-ray™ discs.

Renesas Electronics' new EMMA 3TJ and EMMA3TS SoCs facilitate the development of TVs, STBs and digital broadcast receiver modules for markets including Japan and South America, where adoption of the ISDB-T terrestrial digital broadcast format has been spreading in recent years.

The company intends to market the new SoCs aggressively and aims to expand its sales in the South American market to approximately 10 billion yen in 2013 by increasing its accompanying lineup of high-performance digital AV product offerings.

Pricing and Availability

Samples of Renesas Electronics' new EMMA3TJ and EMMA 3TS SoCs are scheduled to be available in the fourth quarter 2010 with each pricing starting at $39 per unit. Mass production is scheduled to begin by December 2010 and is expected to reach a combined volume of 300,000 units per month.
(Pricing and availability are subject to change without notice.)

Please refer to the separate sheet for the main specifications of Renesas Electronics' new EMMA3TJ and EMMA3TS SoCs.

(Remarks)
EMMA is a trademark or registered trademark of Renesas Electronics Corporation in Japan, the United States, and other countries. Blu-ray is a trademark of the Blu-Ray Disc Association. MIPS32 and MIPS32 4KEc are registered and/or trademarks of MIPS Technologies, Inc. Other names of products and services mentioned in this text are the trademarks or registered trademarks of their respective owners.

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723), the world's number one supplier of microcontrollers, is a premier supplier of advanced semiconductor solutions including microcontrollers, SoC solutions and a broad range of analog and power devices. Business operations began as Renesas Electronics in April 2010 through the integration of NEC Electronics Corporation (TSE:6723) and Renesas Technology Corp., with operations spanning research, development, design and manufacturing for a wide range of applications. Headquartered in Japan, Renesas Electronics has subsidiaries in 20 countries worldwide. More information can be found at www.renesas.com.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.


End of content

Back To Top