Skip to main content
Renesas Electronics Corporation - June is Pride Month, a month to raise awareness of the rights and the culture of the LGBTQ+ community

Overview

Description

This simulator product makes source level debugging of applications possible in the Renesas integrated development environment, or the High-performance Embedded Workshop, while the target system is not available on hand.

The simulator debugger's exclusive functions (high-function debugging) permits the programs written in C/C++ language or assembly language to be debugged efficiently while the actual MCU is not available on hand.

  • High-accuracy simulation (Cycle accurate)
  • Simulated I/O function (Standard and file input/output functions usable)
  • Virtual interrupt function (Simulation of interrupt operations possible.Virtual interrupts using arbitrary timing and break conditions.Timer module based internal interrupts possible.)

Furthermore, an intuitively understandable easy GUI (graphical user interface) provides a comfortable debug environment.

This product is included in theC/C++ Compiler Package for H8SX, H8S, H8 Family. When the compiler package is installed, the functions of this simulator debugger are added to the High-performance Embedded Workshop environment.

Features

  • Since the simulator/debugger runs on the host computer, the user can start debugging the program while the actual MCU is not available on hand. This will result in a reduced development period of the entire system.
  • The number of instruction execution cycles is calculated by simulating. This enables performance evaluation even in the absence of the actual MCU.
  • The functions outlined below are available, which permit program test and debug to be proceeded efficiently.
    • Support each CPU in the H8SX, H8S, and H8 Families.
    • If an error occurs while the program under debug is running, the user can choose to continue ignoring the error or stop the program.
    • Get profile data and measure performance one function at a time.
    • Comprehensive break functions (virtual interrupt operations also possible).
    • Set and edit memory map.
    • Display a history of function calls.
    • Display C/C++ and assembler source level coverages.
    • Visual debug function based on image and waveform display.
  • The simulator/debugger runs under Windows, allowing breakpoints, memory map, performance and trace to be set in dialog boxes. The environment setup suitable for the memory map of each MCU in the H8SX, H8S, and H8 Families can also be set in a dialog box.
  • Learn More

Release Information

Latest Ver.: V.5.09.00
Released: Jun 7, 2010

Details of upgrade (See Tool News)
Operating Environment

Notes

  • If the High-performance Embedded Workshop V.4.07.00 has not already been installed in your PC, the simulator debugger for the H8SX, H8S, and H8 families cannot be updated to V.5.09.00. So be sure to update your High- performance Embedded Workshop to V.4.07.00 at first.
  • When you run the compiler on Windows 7, update it and then update your High-performance Embedded Workshop to V.4.08.00. For how to update High-performance Embedded Workshop to V.4.08.00, see "High-performance Embedded Workshop Revised to V.4.08.00 (PDF | English, 日本語)".

Target Devices

Downloads

Documentation

Additional Details

Functions

  • Work efficiency is increased, thanks to builder and debugger integration. (Note1)
  • ELF/DWARF2 object formats are supported.
  • Number of execution cycles and the number of calls are graphically displayed one function at a time.
  • The stack is traced.
  • Object optimization is possible by drawing on the information that is output by the profile function.
  • Comprehensive breakpoint functions are supported (virtual interrupt operations also possible). (Note1)
  • Assembler source level coverage display. (Note1)
  • Visual debug function based on image and waveform display. (Note1)

Note

  1. This function is supported in the H8SX, H8S and H8 family simulator debuggers 4.0 or later that are supplied with the H8SX, H8S and H8 family compiler packages V5.0.
Image
Basic simulation function

Basic Simulation Function

Image
Simulated I/O function / Virtual interrupt function

Simulated I/O Function / Virtual Interrupt Function

Image
Image display window

Image Display Window

Image
Waveform display window

Waveform Display Window

Simulation Range

[Functions Supported by this Simulator Debugger]

  • All executable instructions
  • Exception handling
  • Registers
  • Entire address space
  • Peripheral functions listed below in Table 1
Table 1. Peripheral Functions Supported by Each Simulator Debugger
SimulatorModeSYSCR registersTimer
H8/300 Simulator 
H8/300L Simulator 
H8/300HA SimulatorAdvanced
H8/300HN SimulatorNormal
H8S/2600A SimulatorAdvancedlenspanorama_fish_eye
H8S/2600N SimulatorNormallenspanorama_fish_eye
H8S/2000A SimulatorAdvancedpanorama_fish_eye
H8S/2000N SimulatorNormalpanorama_fish_eye
H8SX Normal SimulatorNormallenspanorama_fish_eye
H8SX Advanced SimulatorAdvancedlenspanorama_fish_eye
H8SX Maximum SimulatorMaximumlenspanorama_fish_eye

lens Supported | panorama_fish_eye Partly supported | — Unsupported

[Functions Not Supported by this Simulator Debugger]

  • Dual-ported RAM
  • Pulse width modulator (PWM)
  • Serial communication interface (SCI)
  • A/D converter
  • I/O ports
  • Interrupt controller

Note: Use an emulator to debug these functions.

Support

Knowledge Base

  1. Windows may be destabilized by using a simulator debugger

    There were some cases when WindowsR98 was used. Please update WindowsR98 by using Windows 98 with Service Pack 1.

    Sep 10, 2007
  2. How to set the offset to download an absolute file (*.abs) in High-performance Embedded Workshop when the debugger is connected

    ... do so, use the following procedure. When you connect the debugger, go to [Download modules] in the workspace window. Right click on Absolute file (*.abs) and select [Properties].Set offset to 0, check [Download debug information only] and execute download.Right click on [Download modules] in the workspace window, and ...

    Apr 26, 2017
  3. How to execute the command code to run a batch file?

    ... recognized. Change the file path specification method as shown below, according to whether TCL (Tool Command Language) is Enable/Disable. When TCL is disable, and>tcl(ret)>tcl disable>FL "C:¥Program Files¥Renesas¥tutorial.abs"  When TCL is enable, and>tcl(ret)>tcl enable>FL ¥"C:¥¥Program Files¥¥Renesas¥¥tutorial.abs¥"

    Oct 19, 2009
View All Results from Knowledge Base (11)
Support Communities

Support Communities

Get quick technical support online from Renesas Engineering Community technical staff.
Browse Articles

Knowledge Base

Browse our knowledge base for helpful articles, FAQs, and other useful resources.
Submit a Ticket

Submit a Ticket

Need to ask a technical question or share confidential information?