|



|
 |
 |
|
|
 |
|
 |
Renesas Technology Releases SuperH™ Family SH7652 Offering Industry-First Support for Both IP Broadcasting and DTCP-IP Copyright Protection
− On-chip Ethernet controller, enabling simultaneous 2-channel network
transmission of HD (High Definition) digital content −
Tokyo, November 15, 2006 −− Renesas Technology Corp. today
announced the 32-bit SuperH*1 Family SH7652 microprocessor with an
on-chip Ethernet controller, incorporating the industry’s first
encryption/decryption functions supporting both the copyright protection
function for IP broadcasting*2 will start in Japan, and the
DTCP-IP*3 copyright protection standard for in-home distribution,
for use in digital audiovisual and office automation devices with built-in
network functions. Sample shipments will begin in January 2007 in
Japan.
As enhancements to current 133 MHz SH7650 with DTCP-IP functions, the SH7652
features the addition of a copyright protection function for IP broadcasting in
Japan, a more comprehensive range of peripheral functions, and a 50% increase
in operating speed to 200 MHz.
The SH7652 offers the following features.
| (1) |
IP broadcasting copyright protection, DTCP-IP for in-home distribution, and
other copyright protection support functions plus Ethernet connection functions
in a single-chip, enabling secure network transmission of HD digital
content |
| |
The SH7652 includes an error correction function and encryption/decryption
circuitry for decrypting IP broadcasting content, as well as functions
compliant with the DTCP-IP standard used for content distribution within the
home. These copyright protection authentication functions and content
encryption/decryption functions are implemented using firmware to be provided
together with the SH7652. These functions enable copyright protection
processing and network processing to be handled by a single chip without
further the host CPU burden. Moreover WM DRM10*4 copyright
protection is also supported. |
| (2) |
High-speed Ethernet controller, enabling simultaneous 2-channel
transmission of HD digital content |
| |
An IEEE802.3 standard*5 compliant media access controller
(MAC)*6 is incorporated, enabling connection to a 10/100 Mbps
(megabit per second) Ethernet LAN. The improved processing performance makes it
possible to perform IP broadcasting copyright protection processing and DTCP-IP
control, and carry out simultaneous 2-channel transmission of HD digital
content. |
| (3) |
Comprehensive interface functions, including USB, SD Memory
Card*7, and serial sound interfaces |
| |
A USB 2.0 High Speed compliant USB Host/Function module and SD Memory Card
host interface are included, enabling connection to a memory card and wireless
LAN module. Serial sound interfaces are also incorporated, allowing
playback of MP3, WMA (Windows Media® Audio), and similar audio data well within
the capacity of the high-performance CPU. |
The SH7652 can easily be connected to another microprocessors or CPU
via an on-chip host interface function. This function enables a main
microprocessors performing system control to handle the SH7652 as an
SRAM-equivalent device in performing data transmission and reception.
This allows control as an Ethernet controller, enabling network related
function development to be carried out independently, and simplifying user
product development.
< Development Background >
Progress has been made in connecting digital home appliances compliant with
DLNA*8 standard to a home network. Moreover, the
inauguration of a digital broadcasting service dubbed IP broadcasting is
planned in Japan, and the start of digital content distribution inside and
outside the home will begin.
Meanwhile, authentication and content encryption processing between devices are
essential when transferring copyright protected digital content via a network
in order to protect content on the network from unauthorized access.
Renesas Technology previously released SH7650 featuring DTCP-IP content
protection standard for in-home distribution compatible functions and an
Ethernet controller, and has now developed the 32-bit SuperH Family SH7652
incorporating IP broadcasting copyright protection support functions, DTCP-IP
in-home content protection standard compliant functions, and an Ethernet
controller for the market growth.
< Product Details >
The SH7652 incorporates 32-bit SH-2A CPU core with a built-in double–precision
FPU, and an Ethernet controller. With processing power of 480 MIPS
(million instructions per second) at a maximum operating frequency of 200 MHz,
and copyright protection support functions, it is ideal for use in digital
audiovisual and office automation devices with built-in network
functions.
The copyright protection support functions provided in the SH7652 comprise a
hardware encryption/decryption circuit block, and firmware for
encryption/decryption circuit block and content data transfer control.
The SH7652 includes two video stream port channels that enable high-speed
transfer of MPEG-2*9 TS (Transport Stream) and MPEG-2 PS (Program
Stream) format data. These ports can be connected to an MPEG-2
encoder/decoder chip, enabling encrypted data received via a network to be
decrypted, and transferred to an MPEG-2 chip at high speed as MPEG-2 TS format
video data. Also, performing high-speed encryption of content data by
means of the on-chip encryption circuit before transmission via a network makes
it possible to achieve simultaneous secure network transfer of HD digital
content on two channels.
The SH7652 also includes a comprehensive range of peripheral functions.
A single-channel Ethernet controller is provided that facilitates connection to
a 10/100 Mbps Ethernet LAN. This Ethernet controller incorporates an
IEEE802.3 compliant MAC layer, and an accelerator that performs TCP/IP checksum
computations automatically without software intervention, reducing the load on
the CPU.
USB and SD Memory Card host interfaces are also included, allowing connection
to external devices such as an external storage and a wireless LAN
module. An on-chip serial sound interface and I2C bus used by
digital audiovisual and office automation devices simplify system design, while
the provision of a host interface function allows easy connection to a main
microprocessor for user product control or the like. This interface
performs high-speed transfer of data and commands between a main microprocessor
or CPU and the SH7652 via a 16-bit bus. Use of this interface also allows
network connection functions to be developed in parallel with basic user
product functions, enabling development time to be shortened.
These functions enable network processing and multiple copyright
protection supporting to be implemented by a single chip without imposing a
load on the main microprocessor or CPU, and make possible simultaneous two
channels distribution of HD digital content.
The package used is a 240-pin CSP (13 mm × 13 mm).
On-chip debugging functions are provided, and the small, PC card sized E10A-USB
can be used as an emulator.
The SH7652 will be exhibited at "Embedded Technology 2006" being held
at Pacifico Yokohama from November 15 to 17.
Renesas Technology will continue to extend its lineup of products with an
on-chip Ethernet controller, including the provision of models offering faster
CPU performance, wireless LAN support, and enhanced peripheral functions.
| Notes: |
1. |
SuperH is a trademark of Renesas Technology
Corp. |
| 2. |
IP broadcasting in this press release refers to
the distribution of TV broadcasts via the Internet in Japan. The SH7652
comply with a Japanese broadcasting standard at the announcement. |
| 3. |
DTCP-IP (Digital Transmission Contents Protection
over Internet Protocol) is a standard for IP network content protection,
standardized by the DTLA (Digital Transmission Licensing Administrator). The
SH7652 relating to DTCP-IP support functions were developed by Renesas
Technology using technology developed by Hitachi, Ltd. |
| 4. |
WM DRM10 (Windows Multi Media DRM10) is a digital
copyright technology developed by Microsoft Corporation. Microsoft, Windows,
and Windows Media are registered trademarks or trademarks of Microsoft
Corporation of the United States in the United States and other countries. |
| 5. |
IEEE802.3: IEEE802 is the title of an IEEE
(Institute of Electrical and Electronics Engineers) committee for promoting LAN
standardization. IEEE802.3 is a CSMA/CD 10/100 Mbps Ethernet LAN specification
standard. In CSMA/CD (Carrier Sense Multiple Access with Collision Detection),
the presence of a carrier is detected before transmission, and if a collision
is detected during transmission, the system waits for a predetermined time
before restarting transmission. |
| 6. |
MAC (Media Access Control): A lower sub-layer
within the data link layer, stipulating the frame transmission/reception
method, frame format, data error detection, etc. |
| 7. |
An SD Memory Card is a small memory card whose
specification was originally formulated by 3C (Matsushita Electric Industrial
Co., Ltd., Toshiba Corporation, and SanDisk Corporation) and has been
progressively extended by the SDA (SD Card Association). |
| 8. |
DLNA (Digital Living Network Alliance) is an
industry association that sets guidelines for the interconnection of PCs,
digital home electrical products, and so forth. DLNA guidelines are guidelines
for performing interconnection of products in a home network environment
formulated by DLNA. |
| 9. |
MPEG-2 (Moving Picture Experts Group phase 2) is a
video data compression method comprising part of the MPEG standard. |
* Other product names, company names, or brands mentioned are the property
of their respective owners.
< Typical Applications >
The following devices equipped with a network connection function:
- Digital audiovisual devices: DVD recorders, flat-panel TVs, audio systems,
etc.
- Office automation equipment: Printers, etc.
|
< Prices in Japan > *For Reference
|
Product Name (Type Name)
|
Maximum Operating Frequency
|
Package
|
Sample Price [Tax Included] (Japanese Yen)
|
SH7652
(R5S76520B200BG) |
200 MHz |
240-pin CSP
(13 mm × 13 mm) |
2,000 |
< Important Note >
A license must be obtained from the DTLA (Digital Transmission Licensing
Administrator) before purchase of this product.
< Specifications >
|
Item
|
SH7652 Specifications
|
| Type name |
R5S76520B200BG |
| Power supply voltage |
1.2 V (internal) / 3.3 V (external) |
| Maximum operating frequency |
200 MHz |
| Maximum processing performance |
480 MIPS (at 200 MHz operation) |
| CPU core |
SH2A-FPU (built-in double?precision floating-point unit) |
| On-chip RAM |
32 kbytes |
| Cache memory |
8-kbyte instruction cache memory, 8-kbyte operand cache
memory
(4-way set associative type) |
| External bus interfaces |
SH local bus controller
| - |
SRAM, SDRAM, ROM directly connectable, PCMCIA interface provided |
| - |
Data bus width: External 8/16/32 bits |
|
Host interface function
| - |
16-bit bus width SRAM type interface |
| - |
Incorporating 2 kbyte x 2 bank buffer RAM |
|
| On-chip peripheral functions |
Copyright protection support functions
| - |
Encryption algorithms (AES/DES/3DES/MUGI): 1-block processing also
possible |
| - |
Hash algorithms (SHA-1/SHA-224/SHA-256) |
| - |
Message authentication code generation (HMAC-SHA-1/HMAC-SHA-224/HMAC-SHA
-256) |
| - |
Dedicated DMA controller with built-in descriptor function × 2
channels |
| - |
TTS (Time stamped Transport Stream) packet analysis |
| - |
ProMPEG type forward error correction function |
|
Video stream interface x 2 channels
| - |
Serial/parallel switching possible |
| - |
MPEG TS and MPEG PS both supported |
|
| Ethernet controller x 1 channel TCP/IP checksum accelerator
function |
| Dedicated Ethernet controller DMAC x 2 channels (1 channel
each for transmission and reception) |
| General-purpose DMA controller x 8 channels |
Serial sound interface (SSI) x 2 channels
| - |
Bidirectional serial transfer |
| - |
Various serial audio formats supported |
|
USB 2.0 Host/Function module x 1 channel
| - |
High Speed/Full Speed/Low Speed supported |
| - |
Hub function supported |
|
SD host interface (SDHI) x 1 channel
| - |
SD memory/IO card interface (1-bit/4-bit SD bus) |
|
| I 2 C bus interface x 1 channel |
Serial communication interface with FIFO (SCIF) x 3
channels
(asynchronous and synchronous serial communication capability) |
| 16-bit compare match timer (CMT) x 2 channels |
| On-chip debugging functions |
| Interrupt controller (INTC) |
| Watchdog timer (WDT) |
| Clock pulse generator (CPG): Built-in multiplication PLL |
| Power-down modes |
Sleep mode |
| Software standby mode |
| Module standby mode |
| Package |
240-pin CSP (13 mm x 13 mm) |
Information contained in this news release is current as of the date of the
press announcement, but may be subject to change without prior notice.
|
|
|
 |