Home /

News Releases 


 
Provide feedback



News Releases


Notices


Press Contacts


Seminars and Events





DOWNLOAD

Renesas Technology Releases 32-Bit SuperH™ Family SH7650 Offering Industry's First Single-Chip Implementation of DTCP-IP Content Protection Standard Compatible Functions


− On-chip Ethernet controller, enabling DTCP-IP standard compatible high definition digital content network transfer with a single chip −



Tokyo, September 1, 2005 −− Renesas Technology Corp. today announced the 32-bit SuperH*1 Family SH7650 microprocessor, incorporating the industry's first DTCP-IP (Digital Transmission Content Protection over Internet Protocol)*2 content protection standard compatible encryption/decryption functions and an Ethernet controller, for use in digital audiovisual and office automation devices with built-in network functions.  Sample shipments will begin in November 2005 in Japan.

The SH7650 offers the following features.

(1) DTCP-IP support functions and Ethernet connection functions in a single-chip, enabling secure network transfer of high definition digital content
The SH7650 includes functions compliant with the DTCP-IP standard. An inter-device authentication function and content encryption/decryption function are implemented by hardware and also by firmware provided together with the SH7650. An IEEE802.3 standard*3 compliant media access controller (MAC)*4 is also incorporated, facilitating the development of a 10/100 Mbps (megabit per second) Ethernet LAN connection function. By this means it is possible to connect a user device to an Ethernet, transfer digital content up to high definition resolution encrypted in real time, and receive, decrypt, and use encrypted content, all with a single SH7650 chip.
In addition, firmware performs DTCP-IP processing automatically when content is transferred. This allows the user to treat such transfers as normal data transfers without having to worry about DTCP-IP processing, simplifying application development. This DTCP-IP related functions and firmware have been produced by Renesas Technology using technology developed by Hitachi, Ltd..

(2) Comprehensive on-chip interface functions including PCI*5 bus controller and host interface
The SH7650 includes a PCI bus controller supporting the widely used PCI standard. Existing inexpensive PC peripheral devices can be used via the PCI bus, enabling system costs to be reduced. In addition, an on-chip host interface (HIF) allows easy connection of the SH7650 to another microprocessor. This function enables the SH7650 to be recognized and controlled by a main microprocessor performing system control in the same way as SRAM, allowing network related function development to be carried out independently, and simplifying user product development.



<Product Background>

More and more home appliances are being connected to a home network. Connecting appliances in the home to a home network makes it possible, for example, for a program recorded on a DVD recorder in the living room to be transferred to and viewed on a DVD recorder or TV set in another room. Among such digital audiovisual devices appearing on the market are models equipped with an Ethernet connection terminal as an Ethernet function, and this trend is expected to increase in the future.

At the same time, it is essential for authentication and encryption processing to be carried out between devices when transferring copyright protected digital content via a network in order to protect content on the network from unauthorized access.

For this market, Renesas Technology has developed the SH7650 32-bit SuperH Family microprocessor incorporating DTCP-IP content protection standard compatible functions and an Ethernet controller.



<Product Details>

The SH7650 incorporates a 32-bit SH-2 CPU core. With processing power of 173 MIPS (million instructions per second) at a maximum operating frequency of 133 MHz, the SH7650 is ideal for use in devices equipped with DTCP-IP content protection standard compatibility and network functions.

DTCP-IP compatible functions provided in the SH7650 comprise a hardware encryption circuit block, and firmware for encryption circuit block and content data transfer control.

Copyright protected digital content transferred via a network must be protected from unauthorized access by means of mutual authentication between devices and content encryption, and it is also necessary for encrypted content to be similarly protected from unauthorized access within the device. The SH7650 includes three MPEG-TS port channels for moving image streaming enabling high-speed transfer of MPEG-2*6 TS (Transport Stream) format data.  These ports can be connected to an MPEG-2 encoder/decoder chip, enabling encrypted data received via a network to be decrypted, and transferred to an MPEG-2 chip at high speed as MPEG-2 TS format moving image data. Also, performing high-speed encryption of content data by means of the on-chip encryption circuit before transmission via a network makes it possible to achieve secure network transfer of digital content including high definition data.

Thus, DTCP-IP support functions are implemented by means of a hardware encryption circuit block and moving image streaming ports, together with firmware (software), as described above.  Having processing performed automatically by firmware makes it unnecessary for the user to directly control DTCP-IP support functions, and enables DTCP-IP compatible content transfer to be performed in the same way as normal network transfer. This firmware is provided together with the SH7650 as a set.

The SH7650 also includes a comprehensive range of peripheral functions.

A single-channel Ethernet controller is provided that facilitates connection to a 10/100 Mbps Ethernet LAN. This Ethernet controller incorporates an IEEE802.3 compliant MAC layer, and an accelerator that performs TCP/IP checksum computations automatically without software intervention, reducing the load on the CPU.

A PCI bus controller is included as an interface to external devices. This allows easy connection to a platform for the PCI bus, which is widely used in home electrical appliances, PCs, office automation equipment, and so forth. An on-chip host interface is also provided, facilitating connection to a main microprocessor for system control or the like. This interface allows recognition of the SH7650 by a main microprocessor as an SRAM-equivalent device, enabling data downloaded via a network to be transferred to the main microprocessor at high speed.

Use of these external interface functions not only allows network connection functions to be developed in parallel with basic user system functions, enabling development time to be shortened, but also facilitates functional upgrading of an existing system through the addition of an Ethernet connection function.

The package used is a 336-pin CSP (17 mm x 17 mm).

On-chip debugging functions are provided, enabling real-time debugging to be carried out at the maximum operating frequency. The small, PC card sized E10A-USB can be used as an emulator.

Renesas Technology will continue to extend its lineup of products with an on-chip Ethernet controller, including the provision of models offering faster CPU performance, wireless LAN support, and enhanced peripheral functions.


Notes: 1. SuperH is a trademark of Renesas Technology Corp.
2. DTCP-IP standard: A standard for IP network content protection, standardized by the DTLA (Digital Transmission Licensing Administrator)
3. IEEE802.3: IEEE802 is the title of an IEEE (Institute of Electrical and Electronics Engineers) committee for promoting LAN standardization. IEEE802.3 is a CSMA/CD 10/100 Mbps Ethernet LAN specification standard. In CSMA/CD (Carrier Sense Multiple Access with Collision Detection), the presence of a carrier is detected before transmission, and if a collision is detected during transmission, the system waits for a predetermined time before restarting transmission.
4. MAC (Media Access Control) : A lower sub-layer within the data link layer, stipulating the frame transmission/reception method, frame format, data error detection, etc.
5. PCI (Peripheral Component Interconnect) : A bus specification standardized by the PCI Special Interest Group
6. MPEG-2 (Moving Picture Experts Group phase 2) : A video data compression method comprising part of the MPEG standard

* Other product names, company names, or brands mentioned are the property of their respective owners.



<Typical Applications>

The following devices equipped with a network connection function :
  • Digital audiovisual devices: DVD recorders, flat-panel TVs, audio systems, etc.
  • Office automation equipment: Printers, etc.

<Prices in Japan> *For Reference
Product Name
(Type Name)
Maximum Operating Frequency Package Sample Price
[Tax Included] (Yen)
SH7650
(R4S76500B133BG)
133 MHz 336-pin CSP
(17 mm x 17 mm)
2,500 [2,625]

<Important Note>

A license must be obtained from the DTLA (Digital Transmission Licensing Administrator) when purchasing this product.



<Specifications>
Item SH7650 Specifications
Type name R4S76500B133BG
Power supply voltage 1.5 V (internal) / 3.3 V (external)
Maximum operating frequency 133 MHz
Maximum processing performance 173 MIPS (at 133 MHz operation)
CPU core SH-2
On-chip RAM 8 Kbytes
Cache memory 16 Kbytes (mixed instructions/data, 4-way set associative type)
External bus interfaces SH local bus controller
- SRAM, SDRAM, ROM directly connectable, or PCMCIA interface used
- Data bus width: External 8/16/32 bits
PCI bus controller
- External PCI device connectable with 32-bit bus width
- 33 MHz operation possible
Host interface function
- 16-bit bus width SRAM type nterface
- Incorporating 1 Kbyte x 2 bank buffer RAM
On-chip peripheral functions DTCP-IP support functions
- Encryption module
- Dedicated DMA controller with built-in descriptor function
Moving image stream MPEG-TS port x 3 channels
Ethernet controller x 1 channel
Dedicated Ethernet controller DMAC x 2 channels
TCP/IP checksum accelerator
General-purpose DMA controller x 4 channels
Host interface function (1 Kbyte x 2 banks)
Serial communication interface with FIFO (SCIF) x 2 channels (asynchronous and synchronous serial communication capability)
16-bit compare match timer (CMT) x 2 channels
On-chip debugging functions
Interrupt controller (INTC)
Watchdog timer (WDT)
Clock pulse generator (CPG): Built-in multiplication PLL
Power-down modes Sleep mode
Software standby mode
Module standby mode
Package 336-pin CSP (17 mm x 17 mm)


Information contained in this news release is current as of the date of the press announcement, but may be subject to change without prior notice.