Home / Applications /

Automotive 


 
Provide feedback
Print this page



Automotive


Lead-Free/RoHS


Packages


Quality and Reliability


Software and Tools


System Block Diagrams



 


Feature Articles


RENESAS EDGE
** Latest Issue **

 


Powertrain Applications for Automotive

System solutions with Renesas Semiconductors

Renesas is one of the leading suppliers of semiconductors for powertrain electronics. Products like IGBTs, Power MOS-FETs, CAN-transceivers, voltage regulators and microcontrollers support powertrain applications. Especially in the area of 32-bit microcontrollers with embedded flash, Renesas is a leader in both technology and performance.

Renesas’s roadmaps are based on our long industry experience, and open up future perspectives for even higher performance.

The 32bit microcontroller SH705x family is dedicated for Engine Management Systems. It incorporates specific peripherals for powertrain applications and offers, with the SH7058F, the fastest and largest embedded Flash currently available.

The Challenge - Increasing System Performance Requirements and Greater Memory

Powertrain applications are driven by two goals:

  • Reduced fuel consumption
  • Reduced emissions

Both goals need to be achieved at the same- or even higher- engine power and, of course, at the same system cost level.

Looking at the driving forces we see:

  • Enhancements in application: New systems like Electronic Valve Drive (EVD), Continuous Variable Transmission (CVT) or Integrated Starter-Alternator systems require higher performance and additional code.
  • New communication interfaces: FlexRay, Byteflight or time-triggered CAN need to be managed.
  • New Software requirements will require more code and higher computing power. These include Auto Code Generation, Quality improvements for Software and model based calculations.

As the technological leader in embedded flash, Renesas is well prepared to support these rapidly increasing performance requirements and the demand for greater embedded Flash memory.


Block diagram for Powertrain - A Platform Approach



Powertrain applications have a similar structure, and differ mainly by

  • Microcontroller Performance,
  • Memory Size
  • No. of Inputs / Outputs.

This calls for a platform approach.

Renesas supports this approach with the SH705x microcontroller family that is upwardly-compatible in software, with cores from 10 to 500 MIPS for Automotive and a huge peripheral mix.
The tool chain can be used from the low end up to high end solutions, reducing the development time and for redesign and requalification.


The Commitment - Long Experience and Future Perspectives

Renesas is the No. One worldwide in 32bit microcontrollers with embedded flash for powertrain applications. We are partner to the 12 leading global powertrain suppliers. This underlines our commitment to powertrain applications.

Renesas invests heavily in leading edge technology in order to maintain this position.

Our long term commitment includes

  • a consistent microcontroller roadmap with factor 2 performance and embedded memory size every 2 years
  • SW compatible cores and toolchain
  • Local support
  • Steady and longterm supply
  • Excellent quality and reliability performance
  • Excellent EMC characteristics

The Whole Set - Hardware, Software, System Integration & Support

Powertrain Key Products

Renesas Tools

  • EVB7055

3rd Party Tools

Software