Skip to main content
Renesas Electronics Corporation - June is Pride Month, a month to raise awareness of the rights and the culture of the LGBTQ+ community
This Software / Tool Has Been Discontinued

Please contact technical support with any questions.

Overview

Description

Reasonably priced and packed with special features, E8 products fully support speedy market-entry for the low-cost R8C/Tiny System products. Not only sophisticated various debug features, E8 offers flash memory programming features. [Learn More]

Release Information

E8 Emulator Software

Target Devices

Downloads

Documentation

Additional Details

Successor

E8a

For details of the migration from the E8 to the E8a, refer to "Migration from E8 to E8a" in the E8a Design Support page.

Target Devices

Supported MCUsFunctions Availability
On-chip debuggingFlash memory programming
High-performance Embedded Workshop graphic interfaceHigh-performance Embedded Workshop graphic interfaceFlash Development Toolkit graphic interface
Target Devices for E8 (PDF | English, 日本語)Available MCUs' for Flash Development Toolkit (PDF | English, 日本語)
M16C Family
M32C/80 Serieslenslenslens
M16C/60 Serieslenslenslens
M16C/30 Serieslenslenslens
R8C/Tiny Serieslenslenslens
M16C/Tiny Serieslenslenslens
H8 Family
H8/300H Tiny Serieslenslens

H8/300H Super Low Power Serieslenslens

H8/300L Super Low Power Serieslenslens

740 Family
740 Series (QzROM)

38000 Series (QzROM)

lens

lens Available | — Not Available

Note that flash memory quick programming at the Flash Momory Writing mode included in E8 emulator is available for the M16C and H8 family microcomputers that support the on-chip debug functions in the matrix above.

Support

Support Communities

  1. FDT Serial Port and R8C

    "Hello. I am trying to get FDT 4.09 to work with a USB to RS232 FTDI converter. FDT does not manage any of the ports (RST, DTR, etc.). I gave up!!! I wrote a Python script that controls a real COM port with a USB converter. The script ...

    Apr 25, 2025
  2. Programmer renesas D70F3379

    Dear, Programmer E8a not manage MCU renesas D70F3379? What is the programmer i can use please? Thank you.

    Jun 5, 2021
  3. M30800FCGP Programmer?

    Hi friendscan i use E8a emulator for program M16C/80 MCUs on board?if not which programmer can do this?

    Jul 27, 2011
View All Results from Support Communities (4)

Knowledge Base

  1. ID code error on E1,E20,E8a,E8(discontinued product) with M16C,R8C Family MCUs

    Confirm the following:Make sure the directory, file, or workspace name is composed of ASCII characters only.If the directory, file, or workspace name has multi-byte characters, the ID code may not be set correctly.Use only ASCII characters for the directory, file, or workspace name. If one of ...

    Apr 26, 2017
  2. Dialog of asking for ID code at connection of an emulator with a MCU

    ... completely erased. Therefore, we recommend activating the emulator in "Erase Flash and Connect" mode.M16C and R8C Family MCUsWhen activated in:"Erase Flash and Connect" (E8a/E8(discontinued product)/E7(discontinued product) mode"Keep Flash and Connect" (E8a/E8(discontinued product)/E7(discontinued product) mode"Debugging ...

    Apr 26, 2017