Overview
Description
・Embedded Target supports the new device RL78/F25.
We offer the above tool for co-simulation between the CS+/e² studio integrated development environment from Renesas interlinked with MATLAB® and Simulink® from the MathWorks, Inc. Among other things, this will support the validation of algorithms and model-based development by customers. For more information of this tool related to using evaluation version or purchasing commercial version, please refer to the release information.
Note: MATLAB®, Simulink® are registered trademarks of The MathWorks, Inc.
Features
- Generation of code for verifying algorithms from Simulink models
- Automatic generation of Processor in the Loop Simulation (PILS) environments
- Supported MCU families: RA, RX, RL78
- What Customers Will be able to Do: Verify the functionality of code for target devices/Measure the performance of code for target devices
- Environments for evaluation through PILS are easy to construct from Model in the Loop Simulation (MILS) environments.
- Evaluation by comparing the results of MILS and PILS (back-to-back testing) is simple and reliable.
- Learn More
Release Information
Latest Ver: V6.10.00
Released: Mar 20, 2026
For customer who consider commercial version of the Embedded Target
The Embedded Target is a tool that works with multiple software tools in tandem.
This tool may not work properly under the following conditions.
- MATLAB® versions are not supported by this product.
- Specifications of Renesas MCU (such as small ROM/RAM size)
- When a size of generated codes, which are affected size and complexity of the Simulink® model, is larger than ROM size of the MCU.
- Inability to communicate due to network security settings, etc.
Again, please check operating environments of the Embedded Target carefully.
Note: MATLAB®, Simulink® are registered trademarks of The MathWorks, Inc.
Target Devices
Target Devices
Note
- The Embedded Target may not work properly with certain ROM/RAM size of a device and/or size and complexity of a model.
- When using Embedded Target with an RA family device, an emulator and an actual device are required to perform PILS (Processor In the Loop Simulation). In addition, additional settings are required to match the FSP version and GCC version in use. For more information, refer to FAQ in below.
FAQ: Project cannot be generated when using RA family in Embedded Target. (Embedded Target error code E300) - The FSP installer for RA family is available on GitHub.
See All Versions(GitHub)
Design & Development
Videos & Training
This video will introduce a useful software tool: Embedded Target. It can help developers reduce both testing time and costs in model-based development. Embedded Target can create an automatically configured model for the PILS environment. Next it generates a Renesas IDE project for PILS. Finally, model verification is performed by checking the execution time on an MCU or simulator.
Additional Details
Functionality
- Generation of code for verifying algorithms from Simulink models
- Automatic generation of Processor in the Loop Simulation (PILS) environments
- Supported MCU families: RA, RL78, RX
What Customers Will be able to Do
- Verify the functionality of code for target devices and
- Measure the performance of code for target devices
Other Benefits to Customers
- Environments for evaluation through PILS are easy to construct from Model in the Loop Simulation (MILS) environments.
- Evaluation by comparing the results of MILS and PILS (back-to-back testing) is simple and reliable.
Software License Agreement
Software License Agreement (PDF | English, 日本語)