Skip to main content

The following page content corresponds to the products marketed in Japan.
If you do not live in Japan, please

Touch panel Functions
SuperH-based Platform Incorporates Touch panel Functions to Aid System Development

The new development platform for products that use touch panels is supported by middleware from technology partners and can be customized and produced in volume for final products

Toru Hayakawa
Executive General Manager
System Business Division
Renesas Solutions Corp.

Touch panels for controlling devices such as mobile phones, car navigation systems, copiers, and production equipment are becoming very popular. They provide added value and desirable new features in products that use a variety of graphical user interfaces (GUIs). Unfortunately, the code for implementing touch panel interfaces is complex, causing problems for efforts to shorten software development projects. This article highlights a Renesas touch panel product that helps resolve such schedule difficulties: a new platform that accelerates the development of high-end products that use SuperH™ processors and incorporate a touch panel LCD screen. This platform assists customers by providing a turnkey solution that eliminates some of the design and debug work that would otherwise have to be done in order to create new end products.

Seeing a need for a development platform that provides touch panel control, then meeting that requirement

LCD touch panels have made controlling many different types of electronic products easier — and in some cases, even fun. They have already been applied to great effect in popular consumer products such as mobile phones and car navigation systems, as well as in office equipment (copiers, etc.), production machinery, industrial equipment, and more. Importantly, LCD panels allow the use of innovative graphical user interfaces (GUIs). They add value by making product operation and control more intuitive through the use of features such as animation and 2D and 3D graphics. An additional benefit is that these panels and optimized GUIs can eliminate the need for traditional keypads, switches and knobs, thereby making it possible to simplify and shrink the size of products, especially portable ones.

Unfortunately, existing microcomputer development platforms, evaluation boards, and other resources are not keeping pace with the trend to touch panel use. Most development boards that provide an LCD panel don't have touch panel controls, but instead use on buttons, arrow keys, and so on for control. Therefore, they make it difficult for application developers to experience how a touch panel operates. As a result, system engineers have requested a more comprehensive range of middleware and are seeking a development platform with a design and features that are closer to those of end products that incorporate touch panels.

Recognizing how important it is to offer system development tools that let customers to experiment with and apply all the features and capabilities of our microcomputers, Renesas has long pursued a two-prong strategy to meet market needs. We develop our own solutions, of course. However, we also actively seeking to take advantage of other firms' expertise by collaborating with companies that can provide additional products and services that deliver value to our customers. Thus, support for our devices includes an extensive array of hardware and software tools from Renesas, plus a wide range of tools from the expert suppliers in a large, vibrant global support community.

Customer interest is particularly strong now for middleware and system development platforms. To provide these types of support for applications that use touch panels, Renesas has teamed up with ALGO SYSTEM Co. Ltd. (referred to below as ALGO SYSTEM). The objective of this successful collaboration was to develop the "Platform with Touch panel Function" for touch panel devices (see Photograph 1).

This development platform loads middleware developed by Renesas and its partner companies on a panel computer with a touch panel that was jointly developed by Renesas and ALGO SYSTEM. The platform looks just like an ordinary panel computer, allowing for development to be undertaken in an environment that is closer to that of the end product.

Photograph 1: External view of "Platform with Touch panel Function."

Letting system engineers immediately see the effects of changes made to the GUI

A main benefit of the development platform with the touch panel function is that it significantly shortens the time it takes to create and debug the user interface. System engineers can immediately view the effects of the modifications they make and interact with the revised controls. Examples of typical modifications include changing the on-screen icons, button shapes, and button and tab colors, as well as the background image, while maintaining — or altering — the overall layout and control positions.

During demonstrations of this platform to customers, many of the design engineers quickly became impressed by the big impact of touch panel features such as animation middleware. Their positive reactions confirmed that the "Platform with Touch panel Function" is a good solution for system development. Also, some customers observed that, unlike existing microcomputer development boards, the new platform is very close to an end product. In fact, several of them commented that it could be converted into an actual product with only minimal customization.

This response has prompted ALGO SYSTEM to begin marketing the "Platform with Touch panel Function" as a standard panel computer — the "ALGO Smart Panel" — instead of a development platform. Additionally, the company can manufacture the platform as a product customized to meet specific system design requirements.

As a result of this revised marketing strategy, one could say that the "Platform with Touch panel Function" uses the ALGO Smart Panel as a development tool — a complete role reversal. An advantage of this situation is a significant reduction in the cost of the development kit, demonstration systems, and similar tools compared to previous products. It also has ensured that the platform and its various derivatives can be supplied in large quantities.

Offering versions of the platform that support general-purpose and application-specific SuperH processors

The target market for the "Platform with Touch panel Function" encompasses electronic devices that use a touch panel GUI, so it covers a wide range of applications and market sectors. These include not only automotive products such as car audio and navigation systems with large LCD screens, but also many others. They range from audio-visual (AV) equipment such as digital still cameras, digital video cameras, and hi-fi audio systems, to office equipment such as POS terminals and standard and multi-function color printers.

The Renesas semiconductor products supported by the "Platform with Touch panel Function" are mainly devices in the SuperH series. They include general-purpose RISC microcomputers and application-specific products such as the SH-Navi series and SH-MobileR series (see Figure 1). The platform can run the Linux and T-Kernel operating systems. Sales and support services are available from both Renesas and ALGO SYSTEM (algos@algosystem.co.jp).

Recently, particular emphasis has been put on versions of the "Platform with Touch panel Function" that are fitted with the SH-MobileR2 application processor for mobile devices, among others (see Figure 2). One popular version provides a 7-inch WVGA (800 x 400 resolution) color LCD screen that is driven directly by a 400MHz SH-MobileR2 chip, the SH7723. This platform has 128Mbytes of DDR SDRAM, 16Mbytes of NOR flash memory, 512Mbytes of NAND flash memory, an Ethernet port, a USB 2.0 port, and a 1024 x 1024 resistive touch panel. Despite all these features, its case is only 32mm thick.

A version of the touch panel platform fitted with the SH7764 SuperH family processor for digital audio applications has also been developed (see Figure 3). This product combines the functions needed to test digital audio systems and includes a 2.5-inch hard disk drive (HDD) and a CD-ROM drive. It can be used without further modification to develop digital audio players that can rip songs from a CD and store them on the HDD.

Figure 1: Roadmap for development platforms with touch panel functions.
Renesas intends to expand this product range, emphasizing platforms that use SH-Navi and SH-MobileR processors.

Figure 2: Internal block diagram of development platform with touch panel function.
This version is based on the SH-MobileR2 application processor.

Figure 3: Software structure of turnkey solution for digital audio applications.
The available middleware consists of five elements: the Entier embedded database from Hitachi, CDDB song-properties database from Gracenote Corporation, MCDB song properties database from Media Click Inc., MascotCapsule 3D GUI graphics engine from HI Corporation, and a sound codec from Renesas. The image on the right shows a demo screen-shot from a music player developed using this configuration. The player allows a particular song to be quickly identified and played from a library containing several tens of thousands of titles.

Providing middleware that supports the development platform

A rich suite of GUI middleware products is available for the "Platform with Touch panel Function." These middleware offerings have been developed either by Renesas or its partners and most of them can be licensed directly from Renesas. Here are a few examples of the middleware products now available for the platform:

  • MascotCapsule 3D real-time graphics package — This middleware from HI Corporation can display 3D graphics in real time without the need for a hardware accelerator. It is shown in the screen-shot in Figure 3.
  • GENWARE2 development tool — This middleware from International Laboratory Corporation aids GUI development under Windows. It can generate C/C++ source code from the user's GUI data.
  • Flash Lite 3.0 web content viewer — This version of the Flash-player software made popular on PCs is provided by eSol Co. Ltd. A typical screen is shown in Photograph 2.
  • Photograph 2: Demonstration screen powered by Flash-player technology.
    This system uses the Flash Lite 3.0 web content viewer middleware supplied by eSol Co. Ltd.

    Planning for the future

    Renesas will promote the "Platform with Touch panel Function" as a development kit by progressively adding support for new versions of our SH-MobileR and SH-Navi series processors. We are strengthening our cooperation with ALGO SYSTEM and encouraging semi-custom development of the ALGO Smart Panel touch panel computer.


    End of content

    Back To Top