Application Report
The following page content corresponds to the products marketed in Japan.
If you do not live in Japan, please
| Equipment Designs that Use Ethernet Connectivity | ||
Microcomputers with On-chip Ethernet Support Promote Networking Capabilities in Audio-Visual products and Industrial Equipment | ||
| ||
| Content sharing is increasing the popularity of products with Ethernet functions | ||
Initiatives such as the Digital Living Network Alliance (DLNA, see note 1) are driving progress in the networking of AV equipment such as home appliances, PCs, and mobile devices. The aim is to enable the seamless sharing of music, photographs, video, and other digital content. To enable this content sharing while thwarting piracy, the Digital Transmission Licensing Administrator (DTLA, see note 2) is putting in place standards for technology that will ensure the protection of copyrights of the content used in home networks. Meanwhile, the market for home AV networks is finally ramping up as various different types of digital AV equipment have begun to have widespread use (see Figure 1). Ethernet networking technology is common in computer systems. It has been widely adopted as a means of communication between equipment in industrial applications in Europe and America and is becoming more common in Japanese industrial equipment. It's also a good choice for home AV networks. The rising use of Ethernet-based networking will be a long-running trend as users seek easy connectivity and maintenance throughout an entire plant, an office building or a home. Ethernet allows network users to standardize and simplify their infrastructures, including the bus and the network interfaces to each device (see Figure 2). | ||
| ||
| ||
| Requirements for Ethernet microcomputers are addressed by various solutions | ||
Renesas is contributing to applications in the AV, industrial and other market sectors by extending the number and types of our microcomputers that offer integrated Ethernet support functions (see Figure 3). These devices will be called Ethernet microcomputers in the discussion that follows, which describes various features incorporated into Renesas devices to meet market demands. Support for content copyright protection Further, the SH7652 microcomputer incorporates the copyright protection function planned for use with IP broadcasting. This means it implements a function for the copyright protection of content transmitted to an in-home IP network via the internet (see Figure 4). Integrated Ethernet PHY Host interface function The host interface function consists of a 16-bit interface bus and two banks of SRAM, each with a 1Kbyte linear address space (2Kbytes, total). The main microcomputer can access this SRAM and perform reading and writing directly. Also data downloaded via the Ethernet link can be transferred to the main microcomputer at high speed. The host interface function includes an HIF boot function. This allows the code that runs on the SuperH devices to be downloaded from the main microcomputer's flash memory, eliminating the need for external flash memory and reducing system cost. Fast Ethernet microcomputers with SH-4A core Ethernet microcomputers for industrial applications For systems that must connect to PCs, PDAs, and other types of equipment, design engineers typically seek microcomputers that offer USB interfaces. Devices that combine both Ethernet and USB features are the SH7670/1/2/3 (SH-2A core, 200MHz operation, and integrated Ethernet MAC and USB) and the H8S/2472 (H8S/2600 core, 34MHz operation, and integrated Ethernet MAC and USB). Support for user development for each of these models includes a range of evaluation boards from Renesas and its various partner vendors. For the SH7670/1/2/3, the M3A-HS71 evaluation board from Renesas Solutions Corporation will soon be released (see Photograph), and core Ethernet drivers and sample USB software are available. | ||
| More solutions for home networks are planned and overseas initiatives are anticipated | ||
In conjunction with its technology partners, Renesas provides DTCP-IP, DLNA, and IPTV middleware for use in our SH-Ether microcomputers (SH7650 and SH7652) for home networks that comply with copyright protection standards. Our marketing strategy is to first build sales among large Japanese AV equipment manufacturers, then grow volume by undertaking initiatives to expand sales overseas. Because there are bright prospects for growth in products and equipment that exploit the benefits of Ethernet connectivity, we plan to continue introducing new Ethernet microcomputers for Japanese and global markets. Moreover, we will also continue to supply a full complement of evaluation resources, as well. | ||
| ||
| ||
| ||
Notes: | ||
Related Content
Vol.13 and earlier
Japan English