The following page content corresponds to the products marketed in Japan.
If you do not live in Japan, please
- Overview
- Further Information
Three-Phase Asynchronous Motor
The three-phase asynchronous motor makes use of the induction principle for converting electrical energy into mechanical energy. A conductor is placed in an electromagnetic field which is then influenced by a force that tries to move it through the magnetic field. In the AC induction motor the magnetic field is placed in the stationary part (stator). The conductors influenced by the electromagnetic force are located in the rotor. The stator usually consists of 3 phase windings displaced 120 electrical degrees apart. When fed by a three-phase alternating current they induce a current in the conductors of the rotor. The interaction of the magnetic field produced by the stator and the current carrying conductors in the rotor causes the rotor to be 'dragged' round by the stator field. Applications: Suggested Renesas MCU Solutions
| ||||||||||||||||||||||||||||||||||||||||||||||||||
|
We are constantly working to improve and add new information to this site. If you do not see the information that you require, then please select the contact us link below to inform us of your request. |
Japan English