Skip to main content

The following page content corresponds to the products marketed in Japan.
If you do not live in Japan, please

Smoke Detector

Overview

Across the most of the world’s regulations now require smoke detectors to be installed in homes, schools, public and commercial buildings. In addition to sounding an audible alarm when a fire breaks out, smoke detectors must also communicate an alarm notification to a remote control location, such as the local fire station. To detect smoke an LED inside the smoke sensor illuminates and measures the current corresponding to the amount of light output by a light receiving sensor. The current is converted to a voltage by an op-amp, and the voltage is read using an A/D converter. The LED inside the sensor illuminates at regular intervals controlled by a timer in order to reduce the power consumption by sampling the smoke volume intermittently.

Renesas’ 78K0/Kx2-L and R8C/Lx Super Low Power MCUs integrate on-chip the peripheral functions necessary for use in smoke detector design, making it possible to reduce the overall product size. Low-voltage operation contributes to extended battery life, which is essential for detectors that must operate over extended periods of time.

System Block Diagram

Recommended Products

Block Semiconductor device Recommended products Features, etc.
Main controller MCU 78K0/Kx2-L 20-pin, low power consumption
H8/38602R Group 32-pin, low power consumption
EEPROM R1EX24xxx Series I2C bus interface *1
R1EX25xxx Series SPI bus interface *2
Op-amp. HA1630xxx Series CMOS low power consumption, small package, low voltage operation
UPC358GR Bi-polar single power, low power consumption, small pakage
MCU peripheral Reset IC RNA519xx Series Variable detection voltage
General use surge absorprtion circuit protection, etc. Zener diode HZMxNB Series 3-terminal (1 device included) face-mount outline
HZU/HZC Series 2-terminal face-mount outline
NNCDxxDA Series High ESD tolerance optimal for use in surge absorption
RDxxS Series 2-terminal face-mount outline
Switching diode HSM2838C、HSM123 3-terminal (2 devices included) face-mount outline
HSU119/HSC119 2-terminal face-mount outline
Schottky diode HRB0502A 3-terminal face-mount outline (low VF)
HRC0103C 2-terminal face-mount outline (low VF, low leak current)
RKR0202AQE 3-terminal face-mount outline (low VF)

*1 I2C: Inter-Integrated Circuit
*2 SPI: Serial Peripheral Interface

■If you do not see the information you need here, please contact us via the link below.

Contact us

PDF version
(recommended for printing)
.


End of content

Back To Top