Skip to main content

The following page content corresponds to the products marketed in Japan.
If you do not live in Japan, please

Pulse Oximeter

Overview

A pulse oximeter is a healthcare product that quickly measures the oxygenation of the blood by using light to monitor the state of the hemoglobin. Recently, such products have become smaller and lightweight and sell at lower prices. As a result, besides being used in the treatment of patients in hospitals, they have become popular for home healthcare and everyday health monitoring, including monitoring during strenuous activities such as mountain climbing or physical exercise.

To perform the oxygen measurement, the meter emits red light and infrared light into the blood, and then detects with a sensor the light that passes through the blood. The signal from the sensor is very weak, so an amplifier circuit is used to raise its level, after which an A/D converter reads the amplified signal. A D/A converter is also necessary to modify the strength of the measuring light to compensate for changes in the level of the ambient light.

MCUs in the 78K0R/Lx3 and R8C/Lx series from Renesas Electronics integrate the on-chip A/D and D/A converters required in pulse oximeters, as well as an LCD drive-control circuit. These on-chip features reduce the number of external components required, making the MCUs ideal choices for pulse oximeter products that must combine compact size and low cost.

System Block Diagram

System Block Diagram

Recommended Products

Block Semiconductor Device Recommended Product Name Features, etc.
Main controller MCU 78K0/Lx3 On-chip LCD driver, low power consumption
R8C/L36x Group
MCU peripheral Reset IC RNA519xx Series Variable detection voltage
General use
surge absorption
circuit protection, etc.
Zener diode HZLxxZ4 Series,
RKZxxKG, KK Series
2-terminal face-mount outline
High ESD tolerance optimal for use in surge absorption
HZMxNB Series 3-terminal (1 device included) face-mount outline
Switching diode HSC/HSD119/HSU119 2-terminal face-mount outline
HSM/HSB2836 Series 3-terminal (2 devices included) face-mount outline
Schottky diode HRC0103C/RER0202 Series 3-terminal face-mount outline (low VF, low leak current)
HRV103B, RKR104BRH low IR, low VF type
RKR0505BKH 3-terminal face-mount outline (low VF)

■If you do not see the information you need here, please contact us via the link below.

Contact us

PDF version
(recommended for printing)
.

Technical Information WEB Magazine RENESAS EDGE


End of content

Back To Top